Highlight Event
Highlight triggers a procedure or calls a script after an object in CimView changes from not highlighted to highlighted.

Field | Description | ||||
---|---|---|---|---|---|
A | Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |||
Procedure | |||||
Script | |||||
B | Parameter | Can be used if the event invokes a script directly or through a procedure. The default code begins as follows. Sub OnHighlight(highlightReason As Long) Where parameters are: | |||
highlightReason | |||||
C | Debounce event | Check | |||
Clear | |||||
Note: When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start.
This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory.
|
Highlight
event is configured for an object, a CimView user can highlight the object by:- Placing the mouse cursor on it.
- Tabbing to it.
- Using the arrow keys to select it.