Dialog Close
Dialog Close triggers a procedure or calls a script when a user closes a screen that was opened using the GefApplication.DialogPopup or GefScreens.DialogPopup method in the CimEdit/CimView GefObject Model.
The event is triggered in the screen that was specified as the parent screen in the DialogPopup call.

Field | Description | ||||
---|---|---|---|---|---|
A | Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |||
Procedure | |||||
Script | |||||
B | Parameter | Can be used if the event invokes a script directly or through a procedure. The default code begins as follows. Sub OnDialogClose(closeReason As Long) Where parameters are: | |||
CloseReason | |||||
C | Debounce event | Check | |||
Clear | |||||
Note: When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start.
This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory.
|
|||||
- GefApplication.DialogPopup method,
- GefScreen.CloseEx method,
- GefScreen.ObjectToEdit property and
- Dialog Close event.