Custom Device
SIS Management: Custom Device Workflow
This workflow describes the process of defining a custom device.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.

Create Custom Device
Persona: Analyst
Create a Custom Device to store the details of the sensor, logic solver, or final element that you want to use.
Select Device from SERH
Persona: Analyst
Select the devices from SERH that make up the custom device. You can create a device with failure rates based on the operating data in your facility. You can also add multiple elements (e.g., valve, solenoid, actuator, quick exhaust) to a device that you plan to reuse in the design of other protective loops.
Provide Device Details and Failure Rates
Persona: Analyst
Provide the custom device details and failure rates.
Approve Custom Device
Persona: Analyst
Approve the custom device so that it can be used in a Protective Instrument Loop.
SIL Verification
Persona: Analyst
Go to the SIL Verification workflow.