Risk Assessment Feature
About the Risk Assessment Feature
The Risk Assessment feature is a combination of:
-
The Risk Assessment window, which is an interface that displays a Risk Matrix and other risk information.
-and-
-
The Risk Matrix data model, which includes entity families, relationship families, and records that determine:
-
The values that you will see in the Risk Assessment interface.
- The calculations that will be performed based on the values that you select.
-
The baseline GE Digital APM database contains a set of baseline records that determine the values that you will see on the Risk Assessment window and the calculations that are performed using those values. You can access this window through modules such as:
- Asset Strategy Management (ASM)
- Asset Criticality Analysis (ACA)
- Risk Based Inspection (RBI)
If you do not want to use the baseline values and calculations, you can customize them or configure your own.
- Asset Strategy Management (ASM)
- Asset Criticality Analysis (ACA)
- Risk Based Inspection (RBI)
Modify the Risk Assessment Window Title
About This Task
You can modify the default title of the Risk Assessment window using the Risk Matrix record.
When you modify the title, the new title will be used everywhere that the Risk Matrix record is used to display the Risk Assessment window. For example, if an Asset Strategy and an RCM Analysis use the same Risk Matrix, if you modify the title in that Risk Matrix record, the new title will be displayed when you access the Risk Assessment interface from any of the following items:
- An Action or Risk in that Asset Strategy
- A Failure Effect or Recommendation in that RCM Analysis.
Procedure
Modify Text Box Labels in the Risk Assessment Window
About This Task
If the default labels Risk Of, Mitigated By, Unmitigated Risk Rank, and Mitigated Risk Rank that appear in the Risk Assessment window are not suitable for your organization and terminology, you can modify the labels using the Risk Matrix record.
When you modify a label, the new label will be used everywhere that the Risk Matrix record is used to display the Risk Assessment window. For example, if an Asset Strategy and an RCM Analysis use the same Risk Matrix, if you modify the labels in that Risk Matrix record, the new labels will be displayed when you access the Risk Assessment interface from any of the following items:
- An Action or Risk in that Asset Strategy.
- A Failure Effect or Recommendation in that RCM Analysis.