Customize the Risk Matrix
About Customizing a Risk Matrix
You can customize the Risk Matrix that appears in the Risk Assessment window throughout GE Digital APM. You can do so by modifying values in the corresponding Risk Matrix record and the records to which it is linked.
You can modify the baseline Risk Matrix record without creating a completely new one, or you can make a copy of the baseline Risk Matrix and customize the copy. Note that only one Risk Matrix record can be specified as the default.
If a Risk Matrix has been used by a module in GE Digital APM, the values in the following fields in the Risk Matrix record cannot be modified:
- Currency
- Use Maximum Risk Rank
- Use Aliases?
- Alias Format Mask
In addition, you will not be able to add or remove probabilities or consequences from the Risk Matrix.
Change the Axis on which Values Appear
About This Task
On the baseline Risk Matrix, values in Consequence records appear on the x-axis, and values in Probability records appear on the y-axis. If desired, you can flip the axes for these families so that values in Probability records appear on the x-axis and values in Consequence records appear on the y-axis.
When you modify the axis setting for one family, the axis setting for the other family is updated automatically to the opposite axis setting. In other words, if you specify that values in Consequence records should appear on the y-axis instead of the x-axis, the axis setting for values in Probability records will automatically appear on the x-axis instead of the y-axis.
Procedure
Change the Order in Which Consequence or Probability Values Appear
About This Task
Procedure
Unlock the Mitigated Consequence
About This Task
By default, the baseline Risk Matrix is configured to lock the mitigated consequence. This means that for mitigated risk assessments, you will be able to modify only the probability value. You will not be able to modify the consequence value.
Procedure
Disable the Not Applicable Check Box
About This Task
In some cases, you might want to disable the Not Applicable check box (which appears on each tab of the Risk Matrix) so that Risk Matrix users cannot select it. For example, your company might have a policy that requires risk to always be evaluated rather than allowing people to bypass the risk assessment process.
Procedure
Hide the Probability and Consequence Names
About This Task
Procedure
Display Custom Values in the Risk Matrix
About This Task
In the baseline Risk Matrix, numeric values appear in each cell in a Risk Matrix. You can hide these numeric values and then use the Use Aliases? option to display aliases in place of the numeric values. For example, instead of the value 1, you could display the alias value Credible - Low.
Procedure
Show the Unmitigated Financial Impact for Each Risk Category
About This Task
The Unmitigated Financial Impact value, stored in Risk Rank records, specifies the estimated monetary value attributed to a specific Risk category. On the baseline Risk Matrix, the Unmitigated Financial Impact value is not displayed by default. These steps describe how to show this value on the Risk Matrix.
Procedure
Change the Financial Precision of the Risk Matrix
About This Task
The Financial Precision value, stored in Risk Matrix records, specifies the number of decimal places to display when rendering financial values in a Risk Matrix. If no Financial Precision value is specified, a Financial Precision of 2 (for example, 1.00) will be used. These steps describe how to change the Financial Precision of a Risk Matrix.
Procedure
Define a Template for Displaying Risk Values
About This Task
If you have decided to display custom values in the Risk Matrix, you can create a template that will determine how values will be displayed in individual cells and on the tab labels.
For example, suppose your custom aliases appear in the Risk Matrix like this:
You can see that the risk value in each cell is a combination of the row alias and column alias, without a delimiter. You can also see that the selected risk value is reflected on the tab label. For instance, at the intersection of the Probable E row and the Very Low 1 column, you see the value E1, which is also displayed on the tab label.
You could change this so that the risk values use a delimiter, such as a dash, so you would see E-1 instead of E1.
Procedure
Create System Codes for a Consequence or Probability Label
Procedure
Specify the Consequence or Probability Label For a Risk Matrix