About This Task
This topic provides detailed instructions on installing the OT Connect Conductor Service using the GE Digital APM Server and Add-ons installer.Note: Re-installing the OT Connect Conductor Service will reset its appsettings.json to the default settings.
Procedure
- On the GE Digital APM Server, access the GE Digital APM distribution package, and then navigate to the \\Setup\Meridium APM Server and Add-ons folder.
- Double-click on the Setup.exe file.
The Welcome window appears.
- Select Next.
The License Agreement window appears.
- Read the License Agreement and, if you agree, select the I accept the terms of the license agreement check box, and then select Next.
The Select Installation Location screen appears.
- Select Next to accept the default location.
The Select the features you want to install window appears.
- Select the OT Connect Conductor Service option.
Note: While additional options are available for selection, these options are not meant to be installed on the GE Digital APM Server at this time. These instructions assume that you want to install only the OT Connect Conductor Service.
- Select Next.
- Select Install.
The Setup Status window appears, displaying a progress bar that shows the progress of the installation process. After the progress bar reaches the end, a message appears, indicating that your server is being configured. After your server is configured, the Installation is Complete window appears.
- Select Finish.
The installation is complete.
Note: The OT Connect Conductor does not require additional configuration. It depends on the common settings in MeridiumAppSettings.xml and Datasources.