GE Digital APM Server First-time Installation
Install the GE Digital APM Server Software and Add-ons
Before You Begin
-
Ensure that your computer meets the hardware and software requirements for the GE Digital APM Server.
- Ensure that you are an administrator with full access to the computer that will serve as the GE Digital APM Server.
- Ensure that the WebDAV Publishing service is deactivated.Important: Before installing the GE Digital APM Server and Add-ons via IIS Manager, the WebDAV Publishing service needs to be deactivated. To verify that it is deactivated, in the Server Manager, in the Roles and Features section of the Local Server workspace, ensure that WebDAV Publishing is not available in the list.
Note:
- Before the installation begins, the installer resets IIS.
- If you want to run the GE Digital APM Server and Add-ons installer in silent mode from the command line, you must ensure that Microsoft .NET Framework 4.7.2 is installed on the GE Digital APM Server. If it is not installed, an error will occur during installation. You can download this program from the official Microsoft website.
- If the GE Digital APM Server and Add-ons installer is run according to the procedure in this topic, and if Microsoft .NET Framework 4.7.2 has not yet been installed on the GE Digital APM Server, it will be installed automatically during the installation.
Procedure
What To Do Next
Install, Repair, or Uninstall
Install, Repair, or Uninstall GE Digital APM Server Components After the Initial Installation.
About This Task
If you need to install a GE Digital APM component on a machine after the initial installation is complete, you can run the GE Digital APM Server and Add-ons installer in modify mode, which will allow you to make changes to the current installation on that machine. Note that the same prerequisites are required when you run the installer in modify mode. You can also run the installer in repair mode to update installed components, or in remove mode to uninstall GE Digital APM components.
Note: IIS will be reset automatically by the installer before the installation process begins.