Inspection Planning Workflow
Inspection Management: Inspection Planning Workflow
This workflow details the process for managing Inspection Profile Items, Inspection Methods, Inspection Tasks, and Work Packs for Execution.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.

Identify Asset for Inspection
Persona: Technician
Depending on the inspection activities to be managed, select the appropriate assets for further definition.
Define Inspection Profile for Asset
Persona: Technician
Define an Inspection Profile to identify what can be inspected and documented during the inspection.
Define Inspection Profile Items
Persona: Technician
Define Inspection Profile Items to identify which individual parts or subcomponents of the asset may be inspected. The Inspection Profile represents the asset inspection configuration, not necessarily what is planned to be inspected for any given task.
Define Inspection Methods?
Persona: Technician
Determine if specific Inspection Methods must be defined to increase the confidence of detection of damage mechanisms.
Define Inspection Methods
Persona: Technician
For each Inspection Profile Item, define specific Inspection Methods (e.g., CUI Inspection, Penetrant Fluorescent Test, Wet Magnesium Particle, and Radiographic X-ray).
Asset Strategy Management
Persona: Analyst
Develop Asset Strategies from various strategy development methods, such as Risk Based Inspection. The actions defined in the strategy are implemented as Inspection Tasks for execution in Inspection Management.
Go to the Asset Strategy Management workflow.
EAM - Work Order Generation
Persona: Analyst
If the overall schedule is being managed by Enterprise Asset Management (EAM), Inspection Tasks may also be created from an EAM work management system.
Go to the EAM - Work Order Generation workflow.
Inspection Tasks Exist?
Persona: Technician
If Inspection Tasks were created from the EAM - Work Management: Work Order Generation workflow, or based on actions from the Asset Strategy Management workflow, then proceed directly to the View Inspection Tasks for Asset step.
Otherwise, proceed to the Create Inspection Task for Asset step.
Create Inspection Tasks for Asset
Persona: Technician
Create Inspection Tasks manually outside of an Asset Strategy for inspection activities that are not managed as part of an overall strategy.
View Inspection Tasks for Asset
Persona: Technician
Irrespective of the initiating means, manage Inspection Tasks to track compliance and inspection activity execution.
Set Up Scope for Inspection Task?
Persona: Technician
Determine if Inspection Tasks should be further defined with specific scope requirements.
Define Inspection Scope for Each Inspection Task
Persona: Technician
Determine and select which of the possible Inspection Methods defined for the Inspection Profile Items of the asset will be carried out for the identified task.
Manage Inspection Tasks by Work Pack?
Persona: Technician
Determine if a group of Tasks will be managed by a Work Pack for work distribution.
If not, then the Inspection Tasks can be performed directly in Inspection Management.
Custom Checklist Template Required?
Persona: Analyst
Determine if the Inspection Tasks require a custom Checklist Template with custom or baseline checklist categories and items.
If not, then the Inspection Tasks can be created using an existing Checklist Template or baseline Inspection families.
Configure Custom Checklist Template
Persona: Analyst
Create a Checklist Configuration Template that includes a custom or baseline assortment of categories and items.
Taxonomy Configuration Required?
Persona: Analyst
Determine if the Checklist Template and/or Baseline Inspection families should be associated only with assets with a specific equipment taxonomy.
If not, the Checklist Template and/or Baseline Inspection families can be used to create Inspection Events for all assets.
Configure Taxonomy Configuration
Persona: Analyst
Create a Taxonomy Configuration that corresponds to equipment taxonomy for the selected asset taxonomy. Link Inspection Families or Checklist Templates to associate them with the assets with that Taxonomy Configuration.
Create an Inspection Work Pack
Persona: Technician
If you will manage Inspection Tasks by a Work Pack, then create an Inspection Work Pack.
Add Inspection Tasks to Work Pack
Persona: Technician
Assign the Inspection Tasks to the Work Pack for work distribution.
Review Inspection Work Pack
Persona: Technician
Review the Work Pack for completeness and accuracy to verify that it is ready to be performed.
Work Pack Ready?
Persona: Technician
Determine if the Work Pack is ready to be performed.
Inspection Assessment
Persona: Technician
If the individual Inspection Task or Work Pack is ready to be performed, then proceed to the Inspection Management: Inspection Assessment workflow.
Go to the Inspection Management: Inspection Assessment workflow.