GAA Wind Events Data Loader
About GAA Wind Events Data Loader
Using the GAA Wind Events Data Loader, you can update the GAA Wind Event.
About the GAA Wind Events Data Loader Requirements
Prerequisites
- Download the GAA Wind Events data loader workbook from the APM Wind Generation data loader category in GE Digital APM.
- Identify the data requirements for exporting data from the Events workspace into the data loader workbook.
- Extract data from the exported Excel file to populate the data loader workbook.Note: Ensure to copy the content from the IEC Events Worksheet.
Security Settings
The user who loads data into GE Digital APM must be associated with the following Security Groups and Security Roles:
-
MI Data Loader User Security Role
or
MI Data Loader Admin Security Role
About the GAA Wind Events Data Loader General Loading Strategy
Best Practices
When using the data loader workbook, consider the following best practices:
- Ensure that Field IDs (that is, row 2 of IEC Events worksheet) do not include special characters or spaces.
- Do not modify the first two rows of IEC Events worksheet once the data to be imported is copied from the exported file.
- Consider the rules described in the Workbook Layout and Use section of this document.
About the GAA Wind Events Data Loader Workbook Layout and Use
Color Coding
Certain columns in the worksheets have different functions and requirements. To illustrate this, they are color-coded. The following table provides a list of colors and what they represent.
Color | Description | Comment |
---|---|---|
Pink | Required fields | Indicates columns that contain values that are required in GAA Wind. |
Blue | Recommended fields | Indicates columns that, according to GE Digital Best Practice for GAA Wind, should contain values. |
White | Optional fields | Indicates columns where you can specify custom fields. |
Configuration Worksheet
Please refer to About the Configuration Worksheet topic that provides a list of fields that appear in the Configuration worksheet.
IEC Events Worksheet
The following table provides a list of fields that appear in the IEC Events worksheet.
Field Caption | Data Type (Length) | Comment |
---|---|---|
Unit Name | Character | Identifies the unit for which Event is reported. |
IEC Type | Character | Identifies the type of the Event. |
Start Date | Date | Identifies the start date of the Event. |
End Date | Date | Identifies the end date of the Event. |
Duration | Numeric | Identifies the difference between the values in the End Date field and the Start Date field. |
Description | Text | Identifies the description of the Event. |
NERC Type | Character | Identifies the NERC equivalent of the IEC type. |
Error Code | Character | Identifies the validation error. |
Actual Production | Numeric | Identifies the actual production of the Unit in megawatt hours. |
Event ID | Character | Identifies the Event. |
Sub Group Key | Numeric | Identifies the key of the Sub Group for which the Event is reported. |
Unit Key | Numeric | Identifies the key of the Unit for which the Event is reported. |
Site Reference Name | Character | Identifies the name of the site that is assigned to the Event record. |
Start Date Timezone | Character | Identifies the name of the time zone for the Start Date field. Note: The value in this field will always be logged in the User time zone. |
End Date Timezone | Character | Identifies the name of the time zone for the End Date field. Note: The value in this field will always be logged in the User time zone. |