Event Types
Access an Event Type
Procedure
- Access the GAA Administrator page.
- In the System Codes section, select Event Types.
The Event Types subsection appears, displaying the following columns of information:
- Event Type Code
- Event Type Description
- Color Code
- Mapped ID
- Regulatory Organization
- Locate the row that contains the Event Type that you want to access.
- In the Event Type Code column, select the link.
The Edit Event Types window appears, displaying the datasheet of the selected Event Type.
Note: As needed, you can modify the values in the available fields, and then selectto save your changes.
Add an Event Type
Procedure
- Access the GAA Administrator page.
- In the System Codes section, select Event Types.
The Event Types subsection appears.
- In the upper-left corner of the Events Types section, select
.
The Add Event Type window appears.
- As needed, enter the values in the available fields.
- Select
.
The new Event Type is added.
Delete an Event Type
About This Task
Important: You must not delete a baseline Event Type.
Procedure
- Access the GAA Administrator page.
- In the System Codes section, select Event Types.
The Event Types subsection appears.
- Select the row containing the Event Type that you want to delete.
- In the upper-right corner of the Events Types section, select
.
The Delete Event Type dialog box appears, asking you to confirm that you want to delete the selected Event Type.
- Select Yes.
The selected Event Type is deleted and the updated list of Event Types appears.