Workflow
European Inspection Management Workflow
About This Task
This workflow provides the basic, high-level steps for using European Inspection Management. The steps and links provided in the workflow do not necessarily reference every possible procedure.
Procedure
Identify an Asset
This topic describes how to identify the certification requirements for the inspectors based on the criticality of the assets.
Procedure
View or Modify Asset Technical Data
This topic describes how to view or modify the Asset Technical Data to determine the certification requirements of the inspectors based on the criticality of the assets.
Procedure
Example
Example: Identify certification requirement for a Pressure Vessel
In this example, two records in Asset Technical Data family are created for the Shell Chamber and the Tube Chamber for the Pressure Vessel asset.
Field | Value for Shell Chamber | Value for Tube Chamber |
---|---|---|
Chamber | Shell | Tube |
Fluid | C1 | C2 |
Fluid Group | 1 | 2 |
Fluid Phase | Gas | Liquid |
Protected Pressure (P) | 50 [Bar] | 30 [Bar] |
Volume (V) | 1200 [Litre] | 500 [Litre] |
Outer Diameter (DN) | This field is blank as values for this field are used for the certification calculation of Asset Type is Piping. | This field is blank as values for this field are used for the certification calculation of Asset Type Piping. |
PV (Protected Pressure*Volume) | 6000 [Bar.Litre] | 15000 [Bar.Litre] |
PDN (Protected Pressure*Outer Diameter) | This field is disabled as the Asset Type is Pressure Vessel. | This field is disabled as the Asset Type is Pressure Vessel. |
Certification | ZUS | BP |
- For Shell Chamber, refer to Reference Table 4 for the certificate calculation.
- For Tube Chamber, refer to Reference Table 5 for the certification calculation.
Certification calculation for Asset type Pressure Vessel for a Shell chamber:

Certification calculation for Asset type Pressure Vessel for a Tube chamber:

Example: Identify certification requirement for a Simple Pressure Vessel
In this example, a single record is created for the Simple Pressure Vessel asset.
Field | Value |
---|---|
Fluid | C2 |
Fluid Group | 2 |
Fluid Phase | Gas |
Protected Pressure (P) | 20 [Bar] |
Volume (V) | 400 [Litre] |
Outer Diameter (DN) | This field is blank as values for this field is used for the certification calculation of Asset Type Piping. |
PV (Protected Pressure*Volume) | 8000 [Bar.Litre] |
PDN (Protected Pressure*Outer Diameter) | This field is disabled as the Asset Type is Simple Pressure Vessel. |
Certification | ZUS |

Example: Identify certification requirement for Piping
In this example, a single record is created for the Piping asset.
Field | Value |
---|---|
Fluid | C3 |
Fluid Group | 2 |
Fluid Phase | Gas |
Protected Pressure (P) | 12 [Bar] |
Volume (V) | This field is blank as values for this field is used for the certification calculation of Asset Type Pressure Vessel, Simple Pressure Vessel, and Steam Boiler. |
Outer Diameter (DN) | 114.3 [mm] |
PV (Protected Pressure*Volume) | This field is disabled as the Asset Type is Piping. |
PDN (Protected Pressure*Outer Diameter) | 1371.6 [Bar.mm] |
Certification | bP |

Example: Identify certification requirement for a Steam Boiler
In this example, a single record is created for the Steam Boiler asset.
Field | Value |
---|---|
Fluid | Test |
Fluid Group | 1 |
Fluid Phase | Liquid |
Protected Pressure (P) | 35 [Bar] |
Volume (V) | 100 [Litre] |
Outer Diameter (DN) | This field is blank as values for this field is used for the certification calculation of Asset Type Piping. |
PV (Protected Pressure*Volume) | 3500 [Bar.Litre] |
PDN (Protected Pressure*Outer Diameter) | This field is disabled as the Asset Type is Steam Boiler. |
Certification | ZUS |

What To Do Next
Apply Suggested Compliance Strategy Templates for an Asset
Users can get suggested Compliance Strategy Templates for assets that are in the Assets without Templates section of the Compliance Management Overview page. This section contains assets that do not have linked Compliance Strategy Templates, but match queries attached to Compliance Strategy Templates.
Before You Begin
Procedure
Results
Create an Inspection Plan from the Compliance Management Overview Page
You can create an Inspection Plan for assets that are linked to Compliance Strategy Templates.
Before You Begin
Procedure
Approve an Inspection Plan
Procedure
Implement an Inspection Plan
Before You Begin
- Ensure that the Implement Recommended Actions to Tasks in ASM setting is set to False in the Inspection Configuration section of the IM Admin Preferences page.
- You must have an Inspection Plan that is in the Approved state.
About This Task
This task describes how to implement an Inspection Plan to an Inspection Task. When you implement an Inspection Plan, all the Compliance Recommendations associated with the Inspection Plan are implemented to an Inspection Tasks.
Procedure
Manage Inspection Tasks
Before You Begin
Ensure that you have implemented an Inspection Plan. For more information on Implementing an Inspection Task, refer to the Implement an Inspection Plan topic.
About This Task
This topic describes how to create and manage a European Inspection Task. The European Inspection Task is introduced to the Inspection Task family to manage the European Inspection tasks, according to the Compliance regulation.
Procedure
Reschedule an Inspection Task
-
Scenario 1: For Completion Date before Compliance Min Date
- Next Date field on Inspection Task is set based on the value in the Completion Date + Desired Interval.
- Task Rescheduling Basis field on Inspection Task will be updated to Next Date based on Last Date.
-
Scenario 2: For Completion Date after Compliance Min Date
- Next Date field on Inspection Task is set based on the value in the Previous Next Date + Desired Interval.
- Task Rescheduling Basis field on Inspection Task will be updated to Next Date based on Next Date.
Field | Last Date (mm/dd/yyyy) | Desired Interval (Months) | Next Date (mm/dd/yyyy) | Compliance Window (Months) | Compliance Min Date (mm/dd/yyyy) | Compliance Max Date (mm/dd/yyyy) |
Value | 02-12-2019 | 36 | 02-12-2022 | 3 | 11-01-2021 | 05-31-2022 |
Behaviour | This is the date in the Inspection Task which will be same as Completion date in Inspection Event. This is a Modifiable field. | The Next Date is updated based on the Last Date + Desired Interval. | Predefined in EU Admin Settings | The date is updated to the First Date of Month for Next Date -Compliance Window | The date is updated to the Last Date of Month for Next Date + Compliance Window |

- Scenario 1: Completion Date in Inspection Event is before the Compliance Min Date in the Inspection Task. Next Date = Last Date + Desired interval
Field Compliance Min Date (mm/dd/yyyy) Completion Date in Inspection Event (mm/dd/yyyy) Last Date (mm/dd/yyyy) Previous Next Date (mm/dd/yyyy) Desired Interval (Months) Next Date (mm/dd/yyyy) Task Rescheduling Basis Compliance Window (Months) Compliance Min Date (mm/dd/yyyy) Compliance Max Date (mm/dd/yyyy) Value 11-01-2021 03-20-2020 03-20-2020 02-12-2022 36 03-20-2023 Next Date Based on Last Date 3 12-01-2022 06-30-2023 Behaviour Compliance Min Date Before Rescheduling As Provided by the user. Same as the Completion Date This was the Next date before Rescheduling Date obtained by adding 36 Months to the Last Date Compliance Min Date After Rescheduling Compliance Max Date After Rescheduling - Scenario 2: Completion Date in Inspection Event is after the Compliance Min Date in Inspection Task. Next Date = Previous Next date + Desired interval
Field Compliance Min Date (mm/dd/yyyy) Completion Date in Inspection Event (mm/dd/yyyy) Last Date (mm/dd/yyyy) Previous Next Date (mm/dd/yyyy) Desired Interval (Months) Next Date (mm/dd/yyyy) Task Rescheduling Basis Compliance Window (Months) Compliance Min Date (mm/dd/yyyy) Compliance Max Date (mm/dd/yyyy) Value 12-01-2022 05-24-2023 05-25-2023 03-20-2023 36 03-20-2026 Next Date Based on Previous Next Date 3 12-01-2025 06-30-2026 Behaviour Compliance Min Date from Scenario-1 As Provided by User Same as Completion Date Next Date from Scenario-1 Date obtained by adding 36 Months to the Previous Next Date Compliance Min Date After Rescheduling Compliance Max Date After Rescheduling
Manage Inspection Events
About This Task
This task describes how to create and manage an Inspection Event. The European Inspection Report is added to the Full Inspection family to manage an Inspection event for an Asset.