Before You Begin
Ensure that the fluid, for which you want to add the fluid properties, is created in the Integrity Fluid Name System Code Table. For more information, refer to the
Create Fluid Records topic.
About This Task
Now, you must add fluid properties for the new fluid added using Record Manager. For more information on Record Manager, refer to the Record Manager documentation. Based on the properties that you define, a group is assigned to the fluid. For more information on the fluid group assignment, refer to Table F of Annexure - 1.Procedure
- Using Record Manager, create a record in the Fluid Data family.
The Fluid Data datasheet appears.

- Enter values in the available fields.
Based on the values, a group is assigned to the fluid.
Note: If required, you can change the default group assigned to the fluid.
- Select
.The fluid properties are added to the fluid record.