Implement Actions
About Implement Actions
In an asset strategy, actions define the work needed to mitigate the risks identified for an asset. That work is executed by implementing the actions, and the method by which you do this depends on the particular action and the GE Digital APM module that is most suitable to use to execute the action.
Consider the following examples:
- If you have an action called Check Lubricant, you may want to implement it by creating a new Lubrication Requirement, which would then be managed in Rounds Designer.
- If you have an action called General Inspection, you may want to implement it with an Inspection Task, whose execution would then be managed in Inspection Management.
- If you have an action with the description Review flow rate, pressure, and vibration for Pump 1, you may want to implement that action with a Health Indicator, which would then be displayed in Asset Health Manager to continuously monitor those items.
In an asset strategy, you can implement an action using one of the following means:
- Calibration Task
- Inspection Task
- Proof Test Task
- Rounds Classic
- Rounds Pro Step
- Lubrication Requirement
- Measurement Location
- Health Indicator
- Policy Instance
In addition, you can:
- Send actions to ASI for SAP, so that they can be implemented and executed in an SAP system.
- Create an EAM Work Request to create alerts that will help you build out a specific EAM structure. When you send the EAM Work Request, a General Recommendation is created in GE Digital APM, which then sends the work request to your EAM system when it is saved.
- View execution history for actions.
Access the Implement Actions Workspace
About This Task
Procedure
About Calibration Tasks
In the Implement Actions workspace, you can create corresponding calibration tasks for actions when you implement the actions. After you create the records, you can link to them from the Implement Actions workspace.
Create New Calibration Task
About This Task
Procedure
Results
- A new calibration task is created.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the calibration task appears.
Link a Calibration Task
About This Task
Procedure
Results
- A new calibration task link is created.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the calibration task appears.
Link Existing Health Indicators
About This Task
In the Implement Actions workspace, you can link health indicator records when you implement the actions. Implementing an action with a health indicator creates a record in Asset Health Management that stores information used to determine the health of an asset.
Procedure
Results
- The health indicator is linked to the action.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the health indicator record appears.
- The Health Status indicator appears on the Strategy Details page of the strategy. The indicator shows the overall status for the asset based on the health indicator diagnostics. The icons used to represent the health statuses are the same used in Asset Health Manager.
About Inspection Tasks
In the Implement Actions workspace, you can create and link corresponding inspection tasks for actions when you implement the actions. After you create the records, you can link to them from the Implement Actions workspace.
Create New Inspection Task
About This Task
Procedure
Results
- A new inspection task is created.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the inspection task appears.
Link an Inspection Task
About This Task
Procedure
Results
- A new inspection task link is created.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the inspection task appears.
About Proof Test Tasks
In the Implement Actions workspace, you can create and link a proof test task for actions when you implement the actions. After you create the records, you can link them to the Inspection task from the Implement Actions workspace.
Create a Proof Test Task
Procedure
Results
- A proof test task is created.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a link to the proof test task appears.
Link a Proof Test Task
Procedure
Results
- A proof test task link is created.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a link to the proof test task appears.
Create New Measurement Location or Lubrication Requirement Records
About This Task
In the Implement Actions workspace, you can create corresponding measurement location and lubrication requirement records to implement an action. After you create the records, you can link to them from the Implement Actions workspace.
Procedure
Results
- A new measurement location or lubrication requirement is created.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the measurement location or lubrication requirement appears.
Link a Policy Instance
About This Task
In the Implement Actions workspace, you can link a policy instance to implement an action. Policy instances are records that identify specific aspects you might want to monitor for an asset, in this case in accordance with actions which have already been identified for the associated asset strategy.
Procedure
Results
- The policy instance is linked to the action.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the policy instance record appears.
Apply Updates to Implemented Actions
Before You Begin
- Modify action(s) as necessary. When you do so, the state assignment for the strategy is changed to Modified.
Procedure
Unlink Implementations
About This Task
Procedure
Link Existing Tasks to Actions
About This Task
In the Implement Actions workspace, you can link calibration and inspection tasks when you implement the actions.
Procedure
Results
- The calibration or inspection task is linked to the action.
- In the Implement Actions workspace, in the Implementation column of the action you implemented, a hyperlink to the calibration or inspection task appears.