Deploy Data Loaders
Upgrade APM Connect Data Loaders to UDLP V2.9.0
This topic outlines the steps that you must complete to upgrade this module to UDLP V2.9.0.
About This Task
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Procedure
Upgrade from any Version DL V1.2.0 through UDLP V2.9.0
Deploy the Data Loaders for the First Time
These are the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic GE Digital APM system architecture.
Before You Begin
About This Task
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are presented.
Configure SSL
If you want to use SSL for connections from APM Connect, this step is required.
About This Task
If you want to use SSL when moving data through the system, you must import security certificates from the secured application into a truststore file accessible to APM Connect. This procedure describes the process for a single application. You can import multiple certificates into a single truststore file by repeating this procedure for each application requiring SSL.
Procedure
Results
Set Permissions for APM Connect Directory
This topic describes the steps for setting up the permissions required to enable the file share.
About This Task
Before you begin importing data into GE Digital APM using the Excel source files, you must set up a network folder share. The data is passed from the APM Server to the APM Connect server through a file share, a situation in which a folder on the network is shared and accessible to both servers.
Procedure
Results
The APM Connect service user has access to the APM Connect folder.
Access Localized Data Loader Workbooks
About This Task
The localized Data Loader workbooks are stored on the GE Digital APM Server.
Procedure
Results
You can access and use the localized workbooks to load data into GE Digital APM. Optionally, you can import the localized workbooks into GE Digital APM so that they can be accessed from the Data Loaders page.
Deploy and Configure Data Loader Files
This topic describes how to access and configure parameters in the context file.
About This Task
Procedure
Deploy and Configure the APM_UPDATE_LOGIC Webservice
The APM_UPDATE_LOGIC webservice manages the temporary tables GE Digital APM uses to load the database. Correct configuration is required for the system to operate correctly.
Procedure
Create the Intermediate Repository Database
This topic describes how to set up a repository in preparation to run your first job.
Before You Begin
- Before you can prepare and deploy the repository, you must import the CreateIntermediateRepository job.
- If you are using the Data Loaders and the EAM Adapters, you must deploy and run the CreateIntermediateRepository job for each set of adapters.
- For SAP adapters, you must first run the Static Data job.
- For multiple EAM systems, the context file parameter values for a specific type of system must be identical except for the value of CMMS_ID.
- For multiple EAM systems, the Intermediate Repository Connection parameters have the same values for all adapters connected to this GE Digital APM system.
Procedure
If you are configuring multiple EAM systems, perform the remaining steps in this topic.