Passive IPLs

About Passive IPLs

A passive IPL can achieve its risk reducing function without the requirement to take any action or change the state of the system. For example, detonation arrestors and blast walls are passive IPLs that reduce the risk.

In LOPA, you can create a Passive IPL record for each type of passive IPL. This record stores the recommended probability of failure on demand (PFD) of the passive IPL device or system. The PFD value indicates the likelihood that the passive IPL system will fail to perform its safety function when required. The Passive IPL records populate the IPL Sub Type field in the IPL Checklist section of the Safeguard, which is of type Passive IPL.

Default Passive IPL Records

By default, the following Passive IPL records are available in APM:

Passive IPL IDLower RangeUpper RangeDefault Value
Blast-wall/Bunker0.0010.010.001
Fireproofing0.0010.010.01
Open Vent0.0010.010.01
Underground Drainage System0.0010.010.01
Flame/Detonation Arrestors0.0010.10.01
Dike0.0010.010.01
Inherently Safe design1E-060.10.01

Access a Passive IPL

Procedure

  1. Access the LOPA Admin page.
  2. In the left pane, select Passive IPL.

    A list of available Passive IPLs appears.

  3. In the Passive IPL ID column, select the link for the Passive IPL that you want to access.

    In the Record Manager, the page for the selected record appears, displaying the datasheet for the record.

    Note: To modify the Passive IPL, as needed, modify values in the available fields, and then select to save your changes. The values in the existing Safeguards that have used the modified Passive IPL will not be affected by the changes. If you want to apply the changes to an existing Safeguard, in the IPL Checklist section of the Safeguard, in the IPL Sub Type box, you must reselect the Passive IPL that you modified.

Create a Passive IPL

Before You Begin

  • For the Passive IPL that you want to create, you must create a System Code in the MI_PASSIVE_IPL System Code Table. The System Code Table populates the Passive IPL ID box. When you create the Passive IPL, in the Passive IPL ID box, you must select the value that you entered in the System Code Table.

Procedure

  1. Access the LOPA Admin page.
  2. In the left pane, select Passive IPL.
    A list of available Passive IPLs appears.

  3. In the upper-left corner of the workspace, select .
    A blank datasheet for Passive IPL appears.

  4. As needed, enter values in the available fields.
  5. In the upper-right corner of the workspace, select .

    The Passive IPL record is created.

Results

Delete a Passive IPL

Before You Begin

Procedure

  1. Access the LOPA Admin page.
  2. In the left pane, select Passive IPL.

    A list of available Passive IPLs appears.

  3. In the row for each Passive IPL that you want to delete, select the check box.

    In the upper-right corner of the workspace, the button is enabled.

  4. Select .

    The Delete Passive IPL dialog box appears, asking you to confirm that you want to delete each selected Passive IPL.

  5. Select OK.

    Each selected Passive IPL is deleted.

Results