Performance Records

About Performance Records

A GAA Wind Performance Record provides information about the GAA Wind Sub Group and performance calculations pertaining to the overall wind turbine operation for a particular month. In addition to calculating the availability and reliability statistics of a wind plant, you can use the record to evaluate the performance of the Sub Group.

 

Access a Performance Record

Procedure

  1. Access the Sub Group Summary page for the Sub Group whose Performance Record you want to access.
  2. Select the Performance tab.

    Performance Records that are associated with the Sub Group appear for each month of the current year, until the current month.



    Tip: To access Performance Records for a different year, use .
  3. Select the link in the row that contains the Performance Record that you want to access.

    The Performance Record page appears.



    Note: As needed, you can modify the values in the available fields, and then select to save your changes.
    Note: You cannot modify a Performance Record when its sync status is OUT OF SYNC unless you regenerate the record.

Access the Performance Record History

About This Task

The history of a Performance Record is recorded each time a field in the record is modified. This topic describes how to access the history of a Performance Record.

Procedure

  1. Access the Performance Record whose history you want to access.
  2. Select , and then select History.

    The Datasheet Field History window appears.

Create a Performance Record

Before You Begin

  • In the Report Configuration record based on which you want to create a Performance Record, ensure that:
    • The Is Report check box is cleared.
    • The Associated Subgroups box contains the Sub Group for which you want to create a Performance Record.
  • Create a Sub Group Capacity record for the Sub Group for the month and year for which you want to create a Performance Record.
  • Import Events for the Sub Group for the month and year for which you want to create a Performance Record.
  • Ensure that the imported Events do not have an error.
  • Ensure that the imported Events do not have a gap in time.
    Note: For a given month and Unit, if the value in the Start Date field of an Event is different from that in the End Date field of the previous Event, the two Events are considered to have a gap in time. In addition, if the Events imported for a given month do not account for all the 24 hours of each day in the month, the Events are considered to have a gap in time.

Procedure

  1. Access the Sub Group Summary page for the Sub Group for which you want to create a Performance Record.
  2. Select the Performance tab.

    The Performance Records that are associated with the Sub Group appear for each month of the current year, until the current month.

    Note: The sync status of a Performance Record that has never been created is OUT OF SYNC.


  3. Select Create Record next to the month for which you want to create a Performance Record.
    The Performance Record page appears. Performance calculations are simultaneously run, and the record is updated.
    Note:

    If the IU time percentage exceeds 2%, a warning message appears to indicate the same. You can, however, create a Performance Record.

    The IU time percentage is the percentage of the total IU time for the Events, as a function of the total report time. For more information, refer to The Data Quality Parameters Window.

    The Events data is considered in the Sub Group timezone for creation of the Performance Record.



Results

The sync status of the Performance Record is SYNCED. If the Event associated with the record is now modified, the sync status will change to OUT OF SYNC.

What To Do Next

Regenerate a Performance Record

Before You Begin

  • Import Events for the Sub Group for the month and year for which you want to regenerate a Performance Record.
  • Ensure that the imported Events do not have an error.
  • Ensure that the imported Events do not have a gap in time.
    Note: For a given month and Unit, if the value in the Start Date field of an Event is different from that in the End Date field of the previous Event, the two Events are considered to have a gap in time. In addition, if the Events imported for a given month do not account for all the 24 hours of each day in the month, the Events are considered to have a gap in time.

About This Task

If the Event associated with a Performance Record has been modified, the sync status of the record will be OUT OF SYNC. You can generate the record again to change the sync status to SYNCED. This topic describes how to regenerate a Performance Record.
Note: You can regenerate a Performance Record only when the sync status is OUT OF SYNC.

Procedure

  1. Access the Sub Group Summary page for the Sub Group whose Performance Record you want to regenerate.
  2. Select the Performance tab.

    The Performance Records that are associated with the Sub Group appear for each month of the current year, until the current month.

  3. Select the row that contains the Performance Record that you want to regenerate.
  4. Select .

    The Regenerate Record window appears, stating that regenerating the Performance Record may take some time.

  5. Select Yes or No as needed.
    Note: Both the Yes and No options in the window will regenerate the Performance Record; however, the Yes option will also update the values in the following fields of the Performance Record, whereas the No option will not:
    • Gross Actual Generation
    • Net Actual Generation
    • Net Maximum Capacity
    Performance calculations are run, and the Performance Record is regenerated.
    Note:

    If the IU time percentage exceeds 2%, a warning message appears to indicate the same. You can, however, regenerate the Performance Record.

    The IU time percentage is the percentage of the total IU time for the Events, as a function of the total report time. For more information, refer to The Data Quality Parameters Window.

    The Events data is considered in the Sub Group timezone for creation of Performance Record.

Results

The sync status of the regenerated Performance Record is SYNCED.

What To Do Next

Delete a Performance Record

About This Task

This topic describes how to delete a Performance Record.

Procedure

  1. Access the Sub Group Summary page for the Sub Group whose Performance Record you want to delete.
  2. Select the Performance tab.

    The Performance Records that are associated with the Sub Group appear for each month of the current year, until the current month.



  3. Select the row that contains the Performance Record that you want to delete.
  4. Select .

    The Delete Record window appears, asking you to confirm that you want to delete the Performance Record.

  5. Select Yes.

    The Performance Record is deleted.

Submit or Resubmit a Performance Record for Review

Before You Begin

  • Ensure that the sync status of the Performance Record is SYNCED.
  • Ensure that you are assigned to at least one of the following Security Roles:
    • MI GAA Wind Super Administrator
    • MI GAA Wind Administrator

About This Task

A Performance Record that is in the In Progress state can be submitted or resubmitted for review. The In Progress state of a Performance Record indicates one of the following:
  • It has never been submitted for review.
  • It has been rejected.
  • It has been re-opened after approval.

This topic describes how to submit or resubmit a Performance Record for review.

Procedure

  1. Access the Performance Record that you want to submit or resubmit for review.
    Note: To know which scenario caused the Performance Record to move to the In Progress state, you can access the History section in the State Assignments window. To access this window, select the In Progress drop-down list box in the Performance Record, and then select the Manage State Assignments option.
  2. Select the In Progress drop-down list box, and then select the Review option, followed by the Done button.
    The Performance Record is submitted or resubmitted for review, and its state is changed to Pending Approval. You can modify the Performance Record.

What To Do Next

Approve or reject the Performance Record.

Approve or Reject a Performance Record

Before You Begin

  • Ensure that the sync status of the Performance Record is SYNCED.
  • Ensure that you are assigned to at least one of the following Security Roles:
    • MI GAA Wind Super Administrator
    • MI GAA Wind Administrator

Procedure

  1. Access the Performance Record that you want to approve or reject.
  2. Select the Pending Approval drop-down list box, and then select the Complete or Reject Review option as needed, followed by the Done button.
    • If you selected the Complete option: The Performance Record is approved and its state is changed to Approved. You can no longer modify the Performance Record.
    • If you selected the Reject Review option: The Performance Record is rejected and its state is changed to In Progress. You can modify the Performance Record.

What To Do Next

Open an Approved Performance Record

Before You Begin

  • Ensure that you are assigned to at least one of the following Security Roles:
    • MI GAA Wind Super Administrator
    • MI GAA Wind Administrator

About This Task

Procedure

  1. Access the Performance Record that you want to open.
  2. Select the Approved drop-down list box, and then select the Reject Completed option, followed by the Done button.
    The Performance Record is opened, and its state is changed to In Progress. You can modify the Performance record.

What To Do Next

Modify the Performance Record, and then resubmit it for review.
Note: If State Management of GAA Wind Performance family is disabled through Configuration Manager, then, the user will not be able to see the state icon in the performance record. But user will be able to perform all the other operations in the performance record and can create its performance report as well. In this case, approval of performance record is not needed for creating performance report.

If State Management of GAA Wind Performance family is enabled again through the Configuration Manager, then, the state will be reset to In-Progress for all the existing performance records.