Catalog Items

Queries Folder

The Catalog folder \\Public\Meridium\Modules\FMEA contains subfolders which contain baseline queries that are used by default in FMEA. The following table identifies the folder locations and results of these queries.

Query

Behavior and Usage

Baseline queries for FMEA in folder \\Public\Meridium\Modules\FMEA
FMEA AnalysisTeamReturns all team members for an analysis. The query is also used to support the FMEA Analysis TeamSub Report report.
RCM FMEA Risks Without Recommendations QueryReturns the list of risks without any recommendations.
Template ListReturns all FMEA templates of the selected template type. The query is used to support the Select Template window of the Apply Template Builder for FMEA.
Baseline queries for FMEA in folder \\Public\Meridium\Modules\FMEA\Analysis
Criticality of RCM FMEA AssetsReturns number of RCM FMEA assets at very high, high, medium, and low criticality.
FMEA Equipment By SystemReturns select equipment records based on Analysis System ID. The query is also used to support the FMEA Analysis Description report.
FMEA FailureModeEffectsReturns analysis details based on function, failure mode, and failure effects. This query is also used to support the FMEA Failure Mode Effects Analysis report.
FMEA Overview Filter QueryDefines the parameters to be used to filter the FMEA Overview page.
FMEA Recommendations by SystemReturns recommendations based on the Analysis System ID. The query is also used to support the FMEA Recommendations report.
Overview Page - FMEA AnalysesReturns all FMEA analyses for the Overview page list.
Overview Page - TemplateReturns all FMEA templates for the Overview page list.

Graphs Folder

The Catalog folder \\Public\Meridium\Modules\FMEA contains the baseline graphs that are used by default in FMEA. The following table contains the graph names and details.

Graph

Behavior and Usage

Percentage of Critical Assets with an AnalysisDisplays a graph representing the percentages of critical assets that have an analysis.
Percentage of Critical Assets an Analysis - LowMediumDisplays a graph representing the percentages of critical assets at low and medium that have an analysis.
RCM FMEA Risks Without RecommendationsDisplays a graph representing the number of risks without recommendations compared to the total number of risks.

Reports Folder

The Catalog folder \\Public\Meridium\Modules\FMEA contains subfolders which contain baseline reports that are used by default in FMEA. The following table identifies the folder locations and descriptions of those reports.

Report

Behavior and Usage

Baseline reports for FMEA in folder \\Public\Meridium\Modules\FMEA

FMEA AnalysisTeamSubReport

SSRS report that is used by the FMEA Analysis Description report.

Baseline reports for FMEA in folder \\Public\Meridium\Modules\FMEA\Analysis
FMEA Analysis DescriptionSSRS report that displays general information for an FMEA analysis, including the associated asset and team members.
FMEA FailureModeEffectsAnalysisSSRS report that displays detailed information of the FMEA analysis, including functions, failures, failure modes, and failure effects.
FMEA RecommendationsSSRS report that displays detailed information of the FMEA recommendations for a system.
Baseline reports for FMEA in folder \\Public\Meridium\Modules\FMEA\SSRS
FMEA Analysis DescriptionSSRS report that displays general information for an FMEA analysis, including the associated asset and team members.
FMEA AnalysisTeamSubReportSSRS report that is used by the FMEA Analysis Description report.
FMEA FailureModeEffectsAnalysisSSRS report that displays detailed information of the FMEA analysis, including functions, failures, failure modes, and failure effects.
FMEA RecommendationsSSRS report that displays detailed information of the FMEA recommendations for a system.

Dashboards Folder

The Catalog folder \\Public\Meridium\Modules\FMEA contains the baseline dashboard that is used for the FMEA Overview page. The following table contains the name of the dashboard and its usage.

Dashboard

Behavior and Usage

FMEA Dashboard

Displays the dashboard for the FMEA module, which contains the All RCM FMEA Risks Without Recommendations and Criticality Distribution of All Assets graphs.