Manual Templates
About Manual Templates
Manual Templates are used to define default values that should appear in a Calibration Template when you perform a manual calibration.
Access a Manual Template
Procedure
- Access the Calibration Admin Preferences page.
- In the pane, select Manual Templates.
The Manual Templates workspace appears, displaying a list of available manual templates.
- In the Template ID column, select the link for the manual template that you want to access.
The selected manual template datasheet appears on a new page, displaying the Calibration Strategy Details and Equipment Details sections. By default, the Calibration Strategy Details section appears.
Note:As needed, you can modify the values in the available fields, and then select .
- If the manual template is not linked to a profile, the changes are saved. For more information, refer to the Manage Calibration Profiles section of the documentation.
-
If the manual template is linked to a Profile, the Update Profiles Using this Template window appears, displaying a list of Asset in the Profile. To update the input and output ranges:
- Select the check box that corresponds to each asset for which you want to update the input and output ranges with those of the manual template.
- Select Update and Save.
The copies of the templates that are linked to the selected Assets are updated with the modified details of the manual template.
Create a Manual Template
Procedure
- Access the Calibration Admin Preferences page.
- In the pane, select Manual Templates.
The Manual Templates workspace appears, displaying a list of available manual templates.
- In the workspace, select , and then select the type of manual template that you want to create.
- Depending on the type of manual template that you selected, enter values in the available fields for the following records:
- Analog Calibration
- Discrete Calibration
- Functional Test
- Multi-Component Analyzer
-
Important: In the Calibration Strategy Details section, the Detail subsection must contain at least one Single Component Analyzer Details record.
- Weight Scale Calibration
- On the page, selects .
The manual template is created.
Delete a Manual Template
Procedure
- Access the Calibration Admin Preferences page.
- In the pane, select Manual Templates.
The Manual Templates workspace appears, displaying a list of available manual templates.
- In the row for each manual template that you want to delete, select the check box.Note: You cannot delete a manual template that is associated with a Calibration Profile.
In the workspace, the button is enabled.
- Select .
The Delete Calibration Template(s) dialog box appears, asking you to confirm that you want to delete each selected manual template.
- Select Yes.
The selected manual template is deleted.