Standard Gas Cylinder and Components

About Standard Gas Cylinder and its Components

A standard gas cylinder is a pressure vessel that stores a mixture of gases of known composition. It is used to calibrate single and multi-component analyzers. The details of a standard gas cylinder and its components are stored in a Standard Gas Cylinder record and Standard Gas Component records, respectively. You must create these records before you calibrate single or multi-component analyzers. Note that for each component in the cylinder, you must create one Standard Gas Component. A Standard Gas Cylinder is linked to each Standard Gas Component through the Has Component relationship.

While creating a Calibration Template for a single or multi-component analyzer, you can link a Standard Gas Cylinder to the template. The APM system creates one Calibration Template Detail record for each component of the cylinder.

Create a Standard Gas Cylinder

Procedure

  1. Access the Calibration Management Overview page.
  2. In the workspace, select the Calibration Tools tab.

    The Calibration Tools section appears, displaying a list of Test Equipments and Standard Gas Cylinders.

  3. In the upper-left corner of the section, select , and then select Standard Gas Cylinder.

    A blank datasheet for the Standard Gas Cylinder appears.

  4. As needed, enter values in the available fields.
  5. In the upper-right corner of the datasheet, select .

    The Standard Gas Cylinder is created.

What To Do Next

Access a Reference Document for a Standard Gas Cylinder

Procedure

  1. Access the Standard Gas Cylinder for which you want to attach a reference document.
  2. Select the Reference Documents tab.

    The Reference Documents section appears, displaying a list of reference documents that are linked to the Standard Gas Cylinder.

    Tip: For more information, refer to the Reference Documents section of the documentation.

Delete a Standard Gas Cylinder

About This Task

Important: Deleting a Standard Gas Cylinder also deletes all the associated Standard Gas Components.

Procedure

  1. Access the Calibration Management Overview page.
  2. In the workspace, select the Calibration Tools tab.

    The Calibration Tools section appears, displaying a list of Test Equipments and Standard Gas Cylinders.

  3. Next to each Standard Gas Cylinder that you want to delete, select the check box.
  4. In the upper-right corner of the section, select .

    The Delete Test Equipment(s) dialog box appears, asking you to confirm that you want to delete the selected Test Equipment.

  5. Select OK.

    The selected Test Equipment is deleted.

Create a Standard Gas Component

Procedure

  1. Access the Standard Gas Cylinder for which you want to create a Standard Gas Component.
  2. In the workspace, select the Standard Gas Components tab.

    The Standard Gas Components section appears, displaying a list of Standard Gas Components.

  3. As needed, enter values in the available fields.
  4. In the upper-right corner of the page, select .

    The Standard Gas Component is created.

What To Do Next

Access a Standard Gas Component

Procedure

  1. Access the Standard Gas Cylinder that is linked to the Standard Gas Component that you want to access.
  2. In the workspace, select the Standard Gas Components tab.

    The Standard Gas Components section appears, displaying a list of Standard Gas Components.

  3. If needed, modify values in the available fields.
  4. In the upper-right corner of the page, select .

    The changes made to the Standard Gas Component are saved.

What To Do Next

Delete a Standard Gas Component

Procedure

  1. Access the Standard Gas Cylinder that is linked to the Standard Gas Component that you want to delete.
  2. Select the Standard Gas Components tab.

    The Standard Gas Components section appears, displaying a list of Standard Gas Components.

  3. In the upper-right corner of the section, select .

    Next to each Standard Gas Component, a check box appears.

  4. Next to each Standard Gas Component that you want to delete, select the check box.
  5. In the upper-right corner of the section, select , and then select Delete.

    The Confirm Delete dialog box appears, asking you to confirm that you want to delete the selected entities.

  6. Select Yes.

    The Standard Gas Component is deleted.