Family Field Descriptions
Checklist Inspection Template Records
The table below provides an alphabetical list and description of the fields that exist for the Checklist Inspection Template family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. See the Site Filtering section of the documentation for more information.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Inspection Family | Character | The family associated with the checklist configuration template. | This field is populated by a list of Inspection Families that contain the Checklist Template field. |
Template JSON | Text | Stores the category configuration for the template as JSON text. |
This field is populated by the application using a JSON structure. This field is populated automatically by the GE Digital APM system. Important: Do not modify the contents of this field.
|
Template Name | Character | Stores the unique name for the template. | This field is populated by the unique name of the Checklist Configuration Template. |
Inspection Records
Inspection records store information about:
- Bundle Inspections
- Bundle Sub-Inspections
- Checklist Inspections
- Full Inspections
- General Inspections
- Inspection Confidence Evaluation
- Pressure Test Inspections
- Pressure Test Sub Inspections
The table below provides an alphabetical list and description of the fields that exist for the Inspection family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Action This Inspection | Character | The action that was performed on the tube bundle during the inspection. | This field displays a list of the IDs and Descriptions of the System Codes that are stored in the MI BUNDLE ACTION (Bundle Sub-Inspection) System Code Table. The value No Action is selected in the list by default. |
Actual Work Time | Numeric | The number of hours required to complete the inspection. | This field appears on datasheets configured for Inspection families whose caption contains the word Checklist and on SAP Integration datasheets configured for the following families:
|
Applicable Regulation | Character | Stores the application regulation for an event | This field is populated with a list of regulations to be linked to a task. This field is populated with a description of system codes stored in MI_INTGY_REGULATION system code table. This field is always disabled. |
As Found Pop Pressure | Numeric | The pressure at which the PRD opens at the time of the inspection. | This field accepts non-negative, numeric values only (for example, 10). |
As Left Pop Pressure | Numeric | The pressure at which the PRD opens after maintenance has been performed on the PRD (for example, cleaning). | This field accepts non-negative, numeric values only (for example, 10). |
Asset ID | Character | The Equipment Record ID to which the Inspection is linked. | This field is populated by the associated Equipment Record ID. This field is populated with either the Equipment Record ID or with the Equipment Record ID that is linked to the selected Functional Location. |
Asset ID Link | Character | A link to the Equipment record to which the Inspection record is linked. | When you select this link, the Equipment record is opened. |
Bundle Inspection Summary | Text | A summary of the inspection. | You can use this field to record any additional information about the inspection that is not stored in another field in the Bundle Sub-Inspection record. |
Bundle Tag | Text | Unique ID applied by the user to identify the bundle. | You can specify a value for this field using the datasheet. |
Bundle Type | Character | The type of the tube bundle equipment. | This field is populated with a list of the IDs and Descriptions of the System Codes that are stored in the MI BUNDLE TYPE (Inspection; Bundle Types) System Code Table. |
Certification | Character | Stores the certification value | The values in this field are populated from a drop-down list box and contains a list of system codes that exist in the MI_COMPLIANCE_STANDARDS system code table. In baseline, the Certification field populates the values which are referenced by MI_INTGY_REGULATION system code table. By default, it shows ZUS and BP. |
Completion Date | Date | The date on which the inspection was completed. | By default, this value is set to the date that the Inspection is created. You can modify this date to reflect the actual completion date. If the value in the Inspection Task Complete field is set to True, the value in the Completion Date field will be used to populate the Last Date field when the Inspection is saved. The commencement date and completion date are always the same. |
Degradation Mechanism | Character | The Degradation Mechanism that was observed during the inspection. | This field displays a list of the IDs and Descriptions of the System Codes stored in the MI DAMAGE MECHANISM (Inspection, Damage Mechanism) System Code Table. The datasheet caption for this field is As Found Degradation Mechanism. |
Deterioration Mode | Character | How the Degradation Mechanism was observed during the inspection. | This field displays a list of the IDs and Descriptions of the System Codes stored in the MI DAMAGE MODE (Inspection, Damage Mode) System Code Table. |
Design Set Pressure | Numeric | The pressure at which the PRD was designed to open. | This field accepts non-negative, numeric values only (for example, 10). |
Downloaded | Boolean | Indicates whether the inspection has been downloaded for field data collection. | This field is set to true when an inspection is downloaded for field data collection. It is set to false when the inspection is synced back. |
Equipment Operating Status | Character | Documents the operating state that the equipment was in at the time of the inspection. | You can specify a value for this field using the datasheet. |
Equipment Technical Number | Character | Unique ID that identifies the equipment. | This ID is assigned during manufacture. |
Extent | Character | The extent to which the inspection was performed. | This field displays a list of values based on the value that you selected in the Type of Inspection field and the values that exist in the Inspection Extent field in Inspection Strategy records. The Extent field displays a list of values that exist in the Inspection Extent field in all Inspection Strategy records whose Inspection Task Type field contains the value that you selected in the Type of Inspection field. |
Filter DM | Boolean | Indicates whether the degradation mechanisms must filter based on the selected RBI component in an Inspection Confidence Evaluation record. | If you select this, the degradation mechanisms are filtered based on the selected RBI component in an Inspection Confidence Evaluation record. This field is enabled only when the Risk Based Inspection license is active and an RBI component is selected in an Inspection Confidence Evaluation record. |
Final Inspection Lock | Boolean | Indicates whether the Inspection record has reached a final state. | Typically, the person reviewing the Inspection Document will set this field to True when the review is complete. When the Final Inspection Lock is set to True, the following fields are disabled:
|
Functional Location ID | Character | The ID of the Functional Location record linked to the Inspection record. | This field is populated with the ID of the Functional Location record with which the Inspection record is associated. This field is either populated by the Functional Location record ID or the Functional Location record of the Equipment record. |
Functional Location ID Link | Character | A link to the Functional Location record to which the Inspection record is linked. | When you select this link, the Functional Location record will be opened. |
Generate Represented Inspections | Boolean | Indicates whether or not Inspection records will be created automatically for equipment in Inspection Groups that you create using the Risk Based Inspection (RBI) module. | When the value in this field is set to True, Represented Inspections may be created. This field is enabled only when the Inspection record fulfills two criteria:
Note: This field is not available in datasheets for the External PRD Checklist and PRD Pop Test Checklist subfamilies. |
Inspection Completion Date | Date | The date on which the inspection was completed. | This field is populated automatically by the GE Digital APM system; however, you can modify the date by selecting ![]() |
Inspection Confidence Evaluation Reviewed | Boolean | Indicates if the Inspection Confidence Evaluation records are reviewed and locked. | You can lock the Inspection Confidence Evaluation records only if:
|
Inspection Document Status | Character | The status of the Inspection Document. | This field displays a list of the IDs and Descriptions of the System Codes stored in the MI STATUS (Status Codes - CORE) System Code table. When an Inspection record is created, the value is set to Draft (DRAFT) by default. You can change it to Pending Approval when you are ready for the reviewer to review it. Likewise, the reviewer can change it to Approved (APPROVED) after they have reviewed it. Note: This field does not apply to Third Party Damage. |
Inspection Document Category | Character | Stores the inspection document category | This field will display a pick list. It will be disabled if Applicable regulation is "European Inspection Regulation" and Certification is "ZUS". If no option is selected or anyone of the option is selected, then the respective field will be enabled. It contains a list of system codes that exist in the MI_EN_DOC_CTGY system code table. The field populates the following values:
|
Inspection Instruction | Character | Stores instructions for the inspector | It contains a list of system codes that exist in the EU_INSP_INST system code table. |
Inspection Headline | Character | A short description of the findings of the inspection. | You can specify a value for this field using the datasheet. |
Inspection Lock | Boolean | Indicates whether the Inspection record is locked. When this field is set to False, the Inspection record is unlocked. When this field is set to True, the Inspection record is locked. | Important: After you lock an Inspection record, only the inspection report owner or team member can unlock it.. When an Inspection record is locked, all fields except for the following fields are disabled:
You can lock an Inspection if you are the Inspection Report Owner or a Contract Inspector who is also a Team Member in the associated Inspection Record. |
Inspection Reference | Character | A value used to identify the Inspection record. | This value is generated automatically by the GE Digital APM system. |
Inspection Report Owner | Character | The first and last name of the GE Digital APM Security User who performed the inspection. | This field contains a list of Security Users who have been assigned the Inspector role. When you create the Inspection record, you must select the name of the GE Digital APM Security User who performed the inspection. |
Inspection Start Date | Date | The date on which the inspection began. | This field is populated automatically by the GE Digital APM system; however, you can modify the date by selecting ![]() |
Inspection Summary | Text | A summary of the inspection. | You can specify a value for this field using the datasheet. |
Inspection Task Complete | Boolean | Indicates whether the Inspection record is closed and the associated Task records have been updated. When this field is set to True, the Inspection record is closed. | When you close an Inspection record:
Note: To modify this check box, you must be assigned the Human Resource role of Inspector. |
Last Downloaded By | Character | The user ID of the resource that downloaded the inspection for field data collection. | This field is set to the user ID of the current user when an inspection is downloaded. |
Last Downloaded Date | Date | The date when the inspection was downloaded for field data collection. | This field is set to the current date when an inspection is downloaded. |
Last Synced Back By | Character | The resource which synced the inspection to GE Digital APM after the field data collection. | This field is set to the user ID of the current user when an inspection is synced to GE Digital APM through Inspection Field Data Collection. |
Last Synced Date | Date | The date when the inspection was synced to GE Digital APM after the field data collection. | This field is set to the current date when an inspection is synced to GE Digital APM through Inspection Field Data Collection. |
Leak Category | Character | The type of leak that is associated with the PRD. | In the datasheet, this field appears as list that contains the following values:
This field is enabled and can retain a value only when the Leak Test Results field contains the value Leak. |
Leak Test Results | Character | Indicates whether there was a leak detected on the PRD during the inspection. | In the datasheet, this field appears as a list that contains the following values:
This list is populated with the descriptions of referenced System Codes for the MI INSP RESULTS LEAK System Code that is stored in the System Code Table with the ID MI RBI REFERENCES. |
No. of Gauges Used | Numeric | The total number of gauges used by a piece of equipment. | You can specify a value for this field using the datasheet. |
Over Pressure Test Results | Character | Indicates whether the PRD passed the Pressure Test that you performed during the inspection. | In the datasheet, this field appears as a list that contains the following values:
|
Percentage Heat Transfer Area Loss | Numeric | The percentage of the area of the tube bundle that will experience heat transfer loss due to plugged tubes. | This value is calculated using the following formula: Percentage Heat Transfer Area Loss = (Total Number of Tubes Plugged At Inspection End / Total Number of Tubes In Bundle) x 100 |
Published | Boolean | Indicates whether the Inspection Document is published. | N/A |
RBI Component | Numeric | The Entity ID of the RBI Component in an Inspection Confidence Evaluation record. | This field displays the RBI Components that are linked to the related asset. If the asset does not have RBI Components, then this list is empty. Based on the value in this field, the degradation mechanisms are filtered in an Inspection Confidence Evaluation record if the Filter check box is selected. This field is enabled only when the Risk Based Inspection license is active. |
Reason for Inspection | Text | The comments from the inspector about why the inspection was performed. | You can specify a value for this field using the datasheet. |
Reviewers Comments | Text | The comments from the reviewer about the Inspection Document. | You can specify a value for this field using the datasheet. Note: This field does not apply to Third Party Damage. |
Reviewers Name | Character | The first and last name of the GE Digital APM Security User who is responsible for reviewing the Inspection Document. | This field contains a list of Security Users who have been assigned the Inspection Supervisor role. When you create the Inspection record, you should specify in this field the Security User who will be responsible for reviewing the Inspection record. |
Scope | Text | The recommended scope for this type of inspection. | This field displays a value based on the value that you selected in the Type of Inspection field, the value that you selected in the Extent field, and the values that exist in the Recommended Inspection Scope field in Inspection Strategy records. The Scope field displays the value that exists in the Recommended Inspection Scope field in all Inspection Strategy records whose:
|
SRV Set Pressure | Text | The pressure at which the test is set. | You can specify a value for this field using the datasheet. |
Tasks Addressed | Character | The tasks that are addressed by the inspection. | You can select Task records associated with the Inspection record from the list of Task Record IDs when you open an existing Inspection record:
|
Test Comments | Text | The comments from the inspector about the performed test. | You can specify a value for this field using the datasheet. |
Test Duration | Numeric | The length of time pressure was held. | You can specify a value for this field using the datasheet. |
Test Media | Text | The liquid or gas used to perform the Pressure Test. | You can specify a value for this field using the datasheet. |
Test Media Temperature | Numeric | The temperature of the test media used. | You can specify a value for this field using the datasheet. |
Test Pressure | Numeric | The pressure at which the test was performed. | You can specify a value for this field using the datasheet. |
Total Number of Tubes in Bundle | Numeric | The number of tubes in the tube bundle. | This value is used to calculate the value in the Percentage Heat Transfer Area Loss field. By default, this field contains the value 0 (zero). If you enter a value in this field, save the record, and then modify the value, the following fields will be populated with the value 0 (zero) because, if you modify the value in the Total Number Of Tubes In Bundle field after saving the record, you should re-enter values in these fields:
The value in this field must be greater than or equal to the:
|
Total Number of Tubes Plugged at Inspection End | Numeric | The number of tubes in the tube bundle that were plugged at the end of the inspection. | This field is populated based on the following values:
|
Total Number of Tubes Replaced at Inspection End | Numeric | The total number of tubes in the tube bundle that have been replaced at the end of a given inspection. | By default, this field contains the value 0 (zero). This field is disabled when the Action This Inspection field contains a value. When the Action This Inspection field contains the value:
|
Tubes (Not Previously Plugged) Replaced | Numeric | The number of tubes in the tube bundle that were not plugged before the inspection started but were plugged during the inspection. | N/A |
Tubes (Plugged At Start) Replaced | Numeric | The number of tubes in the tube bundle that were plugged before the inspection started but were replaced during the inspection. | This field is enabled only when the value in the Action This Inspection field is Partial Retube (PARTIAL RETUBE). This value must be less than or equal to the value in the Tubes Plugged At Inspection Start field. By default, this field contains the value 0 (zero). |
Tubes Plugged at Inspection Start | Numeric | The number of tubes in the tube bundle that were not plugged before the inspection started but were replaced during the inspection. | This field is enabled only when the value in the Action This Inspection field is Partial Retube (PARTIAL RETUBE). By default, this field contains the value 0 (zero). |
Tubes Plugged During This Inspection | Numeric | The number of tubes in the tube bundle that were plugged during the inspection. | This field is enabled only when the Action This Inspection field contains a value other than No Action (NO ACTION). By default, this field contains the value 0 (zero). The value in this field must be less than or equal to the value in the Total Number Of Tubes In Bundle field. When the value in the Action This Inspection field is Bundle Replaced (BUNDLE REPLACED), this field is populated with the value 0 (zero). |
Tubes Plugged in at Inspection Start | Numeric | The number of tubes in the tube bundle that were plugged before the inspection started. | By default, this field contains the value 0 (zero). The value in this field must be:
This value is used to calculate the value in the Percentage Heat Transfer Area Loss field. |
Type of Inspection | Character | The type of inspection that was performed. | This field displays a list of values stored in the Task Type ID field in Task Types records whose Reference field contains the value INSPECTION STRATEGY. The values that appear in this list depend on the type of Inspection record that you are viewing. For Inspection records belonging to:
|
Inspection Recommendation
Inspection Recommendations represent actions that need to be taken as a result of an inspection. The following table provides an alphabetical list and description of the fields that exist in the Inspection Recommendation family.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Alert Assignee When Due? | Boolean | Indicates whether an email notification must be sent to the user selected in the Assigned To Name field when the recommendation is due. | When this check box is selected, the following fields are enabled:
This field appears in the Alert datasheet. |
Asset ID |
Character |
The Equipment Record ID to which the Inspection is linked. |
This field is populated by the Equipment Record ID with which the Inspection record is associated. This field is either populated with the Equipment Record ID, or with the Equipment Record ID that is linked to the selected Functional Location. |
Assigned to Name | Character | The first and last name of the person to whom the recommendation is assigned. |
The value in this field is populated by the First Name and Last Name fields in the corresponding Human Resource records. If the Human Resource record also has an associated Security User, the value from the User ID field also appears. In the database, values in this field are stored in the following formats: <Last Name>, <First Name> ~ <User Name> -or- <Last Name>, <First Name> ~ For example, a name stored in the database would be Smith, Jane ~ jsmith. The Human Resource records that populate the drop-down list box in this field are filtered based on the site that is applied to the Inspection Recommendation. |
Author Name | Character | The first and last name of the person who is proposing the recommendation. |
The value in this field is populated by the First Name and Last Name fields in corresponding Human Resource records that have one of the following roles:
If the Human Resource record also has an associated Security User, the value from the User ID field also appears. In the database, values in this field are stored in the following formats: <Last Name>, <First Name> ~ <User Name> -or- <Last Name>, <First Name> ~ For example, a name stored in the database would be Smith, Jane ~ jsmith. The Human Resource records that populate the drop-down list box in this field are filtered based on the site that is applied to the Inspection Recommendation. |
Business Impact | Character | Records the impact on the manufacturing process during the recommendation implementation. |
This field contains a list of System Codes that exist in the MI BUSINESS IMPACT System Code Table. You can choose from the following baseline values:
|
Completion Comments | Character | Contains notes regarding the completion of the Inspection Recommendation | By default, this field does not contain a value. This field is required if an Inspection Recommendation is superseded. |
Create Work Request? | Boolean | Indicates whether or not a Work Request will be created for the Inspection Recommendation. | N/A |
Days Before Due Date to be Notified | Numeric | The number of days before the Target Completion Date that an email notification must be sent to the user selected in the Assigned To Name field. | This field uses ![]() |
Final Approver Name | Character | The first and last name of the person who is giving the final approval for an Inspection Recommendation. |
The value in this field is populated by the First Name and Last Name fields in the corresponding Human Resource records. If the Human Resource record also has an associated Security User, the value from the User ID field also appears. In the database, values in this field are stored in the following formats: <Last Name>, <First Name> ~ <User Name> -or- <Last Name>, <First Name> ~ For example, a name stored in the database would be Smith, Jane ~ jsmith. The Human Resource records that populate the drop-down list box in this field are filtered based on the site that is applied to the Inspection Recommendation. |
Frequency of Alert After Due Date | Numeric | Specifies how often email messages will be sent after the completion date has passed. | You can choose any of the following options:
This field appears in the Alert datasheet. This field is required when the Alert Assignee When Due check box is selected. |
Functional Location ID |
Character |
The Record ID of the Functional Location record linked to the Inspection record. |
This field is populated with the Record ID of the Functional Location record with which the Inspection Recommendation is associated. This field is either populated by the Functional Location record ID or the Functional Location record of the Equipment record. |
Implementation Alert Text | Character | The text that will be included in the email notification sent to the approver. | This field appears in the Alert datasheet. By default, this field does not contain a value. Optionally, you can type a value in this field. |
Implemented Date | Date | The date on which the Inspection Recommendation was implemented. | N/A |
Inspection Profile Item | Character | The Inspection Profile that represents the subcomponent for which findings are being recorded. | This field is populated with a list of the Inspection Profiles that you have defined for the particular Inspection Scope. |
Mandatory Date | Character | The date on which the Inspection Recommendation must be completed. | N/A This field contains a |
Recommendation Basis | Text | Allows the user to explain the reasoning for why an Inspection Recommendation was proposed. | By default, this field does not contain a value. Optionally, you can enter a value in this field. |
Recommendation Description | Character | A description of the Inspection Recommendation. | By default, this field does not contain a value. Optionally, you can enter a value in this field. |
Recommendation Headline | Character | A short description of the Inspection Recommendation | In the Alert datasheet, if you select the Alert Assignee When Due check box, the value that you provide in the Recommendation Headline field becomes the subject of the alert email. |
Recommendation ID | Character | Unique ID assigned to the Inspection Recommendation. | This field is generated by the GE Digital APM system through business rules. |
Recommendation Priority | Numeric | The priority value used to rank the importance of the Inspection Recommendation. |
N/A This field contains a list of System Codes that exist in the MI_PRIORITY System Code Table. You can choose from the following baseline values:
|
Reevaluate? | Boolean | Indicates whether you want to reevaluate the Recommendation. | This field appears in the Alert datasheet. |
Reevaluation Alert Body Text | Character | The text that will be included in the reevaluation email message. | This field appears in the Alert datasheet. This field is enabled only when the Reevaluate? check box is selected. |
Reevaluation Date | Date | The date on which a reevaluation email message will be sent to the users selected in the Reevaluation Notification List field. | This field appears in the Alert datasheet. This field is enabled only when the Reevaluate? check box is selected. |
Reevaluation Notification List | Text | The first and last name of the person who is notified about reevaluating an Inspection Recommendation. | This field appears in the Alert datasheet. This field is enabled only when the Reevaluate? check box is selected. The value in this field is populated by the First Name and Last Name fields in the corresponding Human Resource records. If the Human Resource record also has an associated Security User, the value from the User ID field also appears. In the database, values in this field are stored in the following formats: <Last Name>, <First Name> ~ <User Name> -or- <Last Name>, <First Name> ~ For example, a name stored in the database would be Smith, Jane ~ jsmith. You can select more than one user in this field. |
Required Equipment Status | Character | Records the operating state of the equipment used to implement the Inspection Recommendation. | N/A This field contains a list of System Codes that exist in the MI_STATUS System Code Table. You can choose from the following baseline values:
|
Reviewer Name | Character | The first and last name of the person who reviewed the Inspection Recommendation. | This field contains a list of Security Users who have been assigned the Inspection Supervisor role. When you create the Inspection Recommendation record, you should specify in this field the Security User who will be responsible for reviewing the Inspection Recommendation record. The Human Resource records that populate this field are filtered based on the site that is applied to the Inspection Recommendation. |
Service Record ID | Character | The ID of the service record. | This field is populated by Service Max when the status of a work request is modified. |
Status | Character | Indicates the status of the Inspection Recommendation as indicated by the user. | This field is populated automatically and set to Created. |
Target Completion Date | Date | The date by which the Inspection Recommendation is intended to be implemented. | This field is required. This field contains a |
Technical Number | Character | A unique ID for the asset to which the recommendation is assigned. | N/A |
Witnessed By | Character |
The GE Digital APM Security User who witnessed the test, which appears in the following format: <Last Name>, <First Name> ~ <User ID> |
N/A |
Work Request Equipment | Character | The equipment against which the work request will be generated. | N/A This field is disabled and populated after the external work request is created. |
Work Request Functional Location | Character | The Functional Location against which the work request will be generated. | N/A This field is disabled and populated after the external work request is created. |
Work Request Reference | Character | The ID of the work request. | N/A |
Inspection Profile
Inspection Profiles represent subcomponents of a piece of equipment on which inspections are performed. The following table provides an alphabetical list and description of the fields that exist in the Inspection Profile family. By default, all fields in the Inspection Profile family appear on the Inspection Profile datasheet.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Item Category |
Character |
The type of subcomponent (e.g., pipes) that exists on the piece of equipment needing inspection. |
This field appears as a list that contains the System Code IDs and Descriptions in the MI INSPECTION PROFILE CATEGORY (Inspection, Profile Category) System Code Table. The Profile Configuration setting determines how this field will be populated. You can modify the value in this field using the datasheet. |
Item Description |
Character |
A description of the subcomponent. |
You can specify a value for this field using the datasheet. |
Item ID |
Character |
The ID of the subcomponent. |
This field is populated automatically based on the value in the Item Category field. You can modify the value in the Item ID field using the datasheet. |
RBI Component |
Character |
The Record ID of the RBI Component that is associated with the Inspection Profile. |
This field appears as a list that contains the Record IDs of all RBI Components that are linked to the associated Equipment. This field is null, by default. This field is enabled only when the Risk Based Inspection license is active. |
RBI Component Family |
Character |
The RBI Component subfamily that is associated with the Inspection Profile. |
This field appears as a list that contains the captions of all RBI Components subfamilies that exist in the baseline GE Digital APM database. This field is populated automatically when you select a value in the RBI Component list. You can modify the selection in this list using the datasheet. |
Sequence |
Numeric |
The order in which the subcomponent should be inspected, relative to other subcomponents on the piece of equipment. |
You can specify a value for this field using the datasheet. |
Inspection Method
Inspection Method records represent the method that will be used to inspect a subcomponent of a piece of equipment that is represented by a linked Inspection Profile record. The following table provides an alphabetical list and description of the fields that exist in the Inspection Method family. All fields in the Inspection Method family, appear on the Inspection Method datasheet by default.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Category |
Character |
The method that should be used to inspect the subcomponent that is represented by an Inspection Profile record to which the Inspection Method record is linked. |
This field appears as a list that contains the System Code IDs and Descriptions in the MI INSPECTION METHOD CATEGORY (Inspection Method Category) System Code Table. The Method Configuration setting determines how this field will be populated. You can modify the value in this field using the datasheet. |
Description |
Character |
A description of the Inspection Method. |
You can specify a value for this field using the datasheet. |
ID |
Character |
The ID of the Inspection Method. |
This field is populated automatically based on the value in the Category field. You can modify the value in the ID field using the datasheet. |
RBI Degradation Mechanism |
Character |
The Potential Degradation Mechanisms record that is associated with the Inspection Method record. |
This field appears as a list that contains the Record IDs of all Potential Degradation Mechanisms records that are linked to the Criticality Calculator RBI Components record that is associated with the Inspection Profile record to which the Inspection Method record is linked. You can specify a value for this field using the datasheet. |
Inspection State Mapping Records
Inspection State Mapping records are used when an administrator uses the Configure Status to State Mapping utility in Application Settings. This topic provides an alphabetical list and description of the fields that exist for the Inspection State Mapping family. The information in the table reflects the baseline state and behavior of these fields.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Source Family | Character | Stores the ID of the family that is being mapped. | The default value for this field is the ID for the Inspection Recommendation family. |
Status | Character | Stores the system code value of the status that is being mapped. The value in this field will be converted to a corresponding state in Inspection Recommendation records. | The values available in this field appear based on the system code table that is associated with the value that populates in the Source Family Status field. |
State | Character | Stores the state ID of the state that is being mapped. The value in this field will be used to replace an existing status in Inspection Recommendation records. | The values available in this field appear based on the available states configured for the source family. |
Inspection Strategy
Inspection Strategies represent methods by which inspections are performed. The following table provides an alphabetical list and description of the fields that exist in the Inspection Strategy family. By default, all fields in the Inspection Strategy family appear on the Inspection Strategy datasheet.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Inspection Confidence |
Character |
A value that indicates how effective prior inspections were at identifying the degradation mechanism and the rate of degradation. |
This field is populated automatically based on the value that you selected in the Type of Inspection field, the value that you selected in the Extent field, and the values that exist in the Inspection Confidence field in Inspection Strategy records. Specifically, the Inspection Confidence field is populated with the value that exists in the Inspection Confidence field in the Inspection Strategy record whose:
This field is not available on the baseline Inspection datasheets. The value that you select in this field is used in RBI when you assign Inspection records to RBI Degradation Mechanism Evaluation records. |
Inspection Extent |
Character |
The extent to which the inspection was performed. |
This field displays a list of values based upon the value that you selected in the Type of Inspection field and the values that exist in the Inspection Extent field in Inspection Strategy records. The Extent field displays a list of values that exist in the Inspection Extent field in all Inspection Strategy records whose Inspection Task Type field contains the value that you selected in the Type of Inspection field. |
Inspection Strategy Description | Character | A description of the Inspection Strategy. | You can specify a value for this field using the datasheet. |
Inspection Strategy ID | Character | The unique ID of the Inspection Strategy. | This field is required. |
Inspection Task Type | Character | The Inspection Method used during the inspection event. | You can specify a value for this field using the datasheet. |
Recommended Inspection Interval | Numeric | The recommended time between inspection events. | You can specify a value for this field using the datasheet. |
Recommended Inspection Scope | Character | An explanation of the tasks that should be performed during an inspection event. | You can specify a value for this field using the datasheet. |
Use Calculated Data | Boolean | Indicates whether or not to use calculated data over data that has been recommended by the GE Digital APM system. | N/A |
Inspection Task
The following table provides an alphabetical list and description of the fields that exist in the Inspection Task family. By default, all fields in the Inspection Task family appear in the Inspection Strategy datasheet.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Applicable Regulation | Character | Stores the regulation type that is applicable to a task. | This field is populated with a list of regulations to be linked to a task. This field is populated with a description of system codes stored in MI_INTGY_REGULATION system code table. This field is always disabled. The value is mapped from Compliance Recommendation. |
Certification | Character | Stores the certification value. | The values in this field are populated from a drop-down list box and contains a list of system codes that exist in the MI_COMPLIANCE_STANDARDS system code table. In baseline, the Certification field populates the values which are referenced by MI_INTGY_REGULATION system code table. By default, it shows ZUS and BP. |
Compliance Window | Numeric | Stores information about the duration of Compliance in months. The UOM is measured in Months. | This field is copied from the Application Settings when a new European Inspection task is created. You can edit the values in the European Inspection Task datasheet. This field is used for calculating the values for the following:
|
Compliance Minimum Date | Date | Mentions the minimum compliance date for a task to be performed. | The Compliance Minimum Date is calculated as the start date of the Next Date minus the Compliance Window (Next Date - Compliance Window). For example: If Compliance Window: 3 months Next Date: December 3rd, 2020 Compliance Min Date: September 1st, 2020 |
Compliance Maximum Date | Date | Mentions the maximum compliance date for a task to be performed. | The Compliance Maximum Date is calculated as the end date of the next date plus the Compliance Window (Next Date + Compliance Window). For example: If Compliance Window: 3 months Next Date: December 3rd, 2020 Compliance Max Date: March 31st, 2021 |
Coverage | Text | A definition of the percentage of the asset to be inspected. | You can specify a value for this field using the datasheet. |
Desired Interval | Numeric | The number of months between inspection events. | N/A |
Desired Interval Basis | Text | The comments from the inspector that explain the reasoning for the selected Desired Interval. | If the value in the Override Interval field is set to True, the value in Desired Interval Basis field will be User-Defined. If the value in the Override Interval field is set to False, the system populates the Desired Interval Basis field with one of the following values:
|
Inspection Documentation Window | Numeric | Stores information about the duration in months for documenting an Inspection report. The UOM is measured in Months. | This field is duplicated from the administrator’s settings when a new European Inspection task is created. You can edit the values in the European Inspection Task datasheet. This field populates values for the Inspection Documentation Completion Date. |
Inspection Documentation Completion Date | Date | Mentions the completion date for documenting an Inspection report. | The value in this field is populated based on addition of Inspection Documentation Window and Compliance Window to the next date. For example: If Inspection Documentation Window: 1 month Compliance Window: 3 months Next Date: December 3rd, 2020 Inspection Documentation Completion Date: April 3rd, 2021 |
Inspection Document Type | Character | The type of document that will be created during Work Pack execution. | N/A |
Last Date | Date | The date on which the last inspection was performed. | This field is populated automatically by the GE Digital APM system; however, you can modify the date by selecting ![]() |
Max Date | Date | The date furthest in the future on which the inspection can be performed and still be in compliance. | This field is populated automatically by the GE Digital APM system; however, you can modify the date by selecting ![]() |
Max Interval | Numeric | The time between the Last Date and the Max Date. | N/A |
Min Date | Date | The earliest date on which an inspection may be performed. | This field is populated automatically by the GE Digital APM system; however, you can modify the date by selecting ![]() |
Min Interval | Numeric | The earliest date on which the inspection can be performed and still be in compliance. | The Desired Interval value must be between the value in this field and that of the Max Interval field. If this field is set to a value that is higher than the Max Interval or Desired Interval, those values are adjusted to be equal to the Min Interval value. |
Modifiable | Boolean | Indicates whether a user can modify fields. | N/A |
Next Date | Date | Date on which the inspection event is schedule. | This field is populated automatically by the GE Digital APM system; however, when the task is reoccurring, you can modify the date by selecting ![]() When an Inspection Task is newly created, this field can be modified when the Last Date field is cleared. |
Next Date Basis | Text | The comments of the inspector; the comments explain the reasoning for the Next Date. | N/A |
Previous Next Date | Date | The date is calculated based on the Inspection Completion date. | This field is populated automatically by the GE Digital APM system. This filed stores the Next Date before the rescheduling occurs. This field is always disabled. |
Override Interval | Boolean | Indicates whether the user may define their own interval. | This field is automatically set to True by the GE Digital APM system; however, you can modify field by clearing the check box. |
Rejectable | Boolean | Indicates whether the inspection task may be rejected and not performed. | This field is automatically set to True by the GE Digital APM system; however, you can modify field by clearing the check box. |
Related Entity ID | Character | The unique ID of that asset that is related to the inspection event. | N/A |
Reoccurring | Boolean | Indicates whether the task is recurring. | This field is populated by Strategy rules, which document the basis of the proposed Next Date. After you save the Inspection Task, you cannot modify the value in this field. |
Source Type | Character | The work process that generated this task. | This field is populated automatically based on the Inspection Scope. |
Task Assigned To | Character | The first and last name of the GE Digital APM Security User responsible for completing the inspection task. | You can enter the name of a Security User in this field. |
Task Description | Text | Defines the requirement for completing this task. | You can specify a value for this field using the datasheet. |
Task Details | Text | A field for the inspector to record additional details about the task. | You can specify a value for this field using the datasheet. |
Task ID | Character | The unique ID used to track the task through the workflow. | This field is required. |
Task State | Character | Indicates to the user the state of the current task. | N/A |
Task Type | Character | The type of inspection that should be performed on the piece of equipment at the interval indicated in the Interval field. | This field is populated with the value that is stored in the Task Type ID field in the Task Types record associated with the time-based inspection setting (that is, the task type for which an inspection interval is defined in the Time-Based Inspection Settings page). |
Task Rescheduling Basis | Character (255) | The rescheduling of the inspection task information is captured in this field. | This field captures the information based on how the Next Date field is calculated. The field can be calculated either by the Completion Date or the Previous Next Date. This field is populated with a description of system codes stored in MI_EU_TASK_RESCHEDULE system code table. This field is always disabled. |
Unconstrain Min/Max Dates | Boolean | Indicates whether the user may define their own min or max dates. | This field is automatically set to True by the GE Digital APM system; however, you can modify field by clearing the check box. |
Inspection Taxonomy Configuration Records
The table below provides an alphabetical list and description of the fields that exist for the Inspection Taxonomy Configuration family. The information in the table reflects the baseline state and behavior of these fields.
This family is not enabled for site filtering, which means that records in this family can be accessed by any user with the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field |
Data Type |
Description |
Behavior and Usage |
---|---|---|---|
Checklist Template | Character | Stores and displays the defined Checklist Configuration Template name. | This field is populated automatically by the GE Digital APM system with the name of a Checklist Configuration Template that has been linked to a Taxonomy Configuration. |
Checklist Template Key | Number | Stores the entity key of the defined Checklist Configuration Template. |
This field is populated automatically by the GE Digital APM system. Important: Do not modify the contents of this field.
|
Inspection Family | Character | Stores the defined Family ID and caption. | This field is populated automatically by the GE Digital APM system with the Family ID and caption of an Inspection Family that has been linked to a Taxonomy Configuration. |
Taxonomy Category | Character | Stores the defined Taxonomy Category. | This field contains a list of available Taxonomy Categories that are available in GE Digital APM. This field can be modified in the Taxonomy Configurations section of Application Settings. |
Taxonomy Class | Character | Stores the defined Taxonomy Class. | This field contains a list of available Taxonomy Classes that are available in GE Digital APM. This field can be modified in the Taxonomy Configurations section of Application Settings. This field is filtered based on the selected Taxonomy Category. |
Taxonomy Type | Character | Stores the defined Taxonomy Type. | This field contains a list of available Taxonomy Types that are available in GE Digital APM. This field can be modified in the Taxonomy Configurations section of Application Settings. This field is filtered based on the selected Taxonomy Category and Taxonomy Class. |
Inspection Team Member Records
Inspection Team Member records contain information for Team Members, such as names and certification information.
An inspection team member is any person that participates in an inspection. When you view an inspection report, you will see a section that lists all team members associated with that inspection.
The table below provides an alphabetical list and description of the fields that exist for the Inspection Team Member family. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Applicable Certification | Character | The relevant certification held by the Team Member. | This field is populated with certifications based on the value in the Full Name field. When you select a Full Name, the certifications associated with that Human Resource appear in the drop-down list box. |
Certification Expiry Date | Date | The date on which the Applicable Certification expires. | This field is populated automatically when you select an Applicable Certification. |
Certification ID | Character | The ID of the Applicable Certification. | This field is populated automatically when you select an Applicable Certification. |
Full Name | Character | The name of the Human Resource for whom the Team Member record is created. | This field is populated by a list of Human Resources who have the Inspector or Contract Inspector role. |
Work Pack
Work Packs store preparation information about inspection work that needs to be performed for equipment and/or locations. The following table provides an alphabetical list and description of the fields that exist in the Work Pack family. By default, all fields in the Work Pack family appear on the Work Pack datasheet.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Preparation Details |
Text |
Preparation information about the inspection work associated with the Work Pack |
You can enter any preparation details about the inspections in this field. |
Work Pack ID |
Character |
The Record ID of the Work Pack |
This is a required field. You must enter a value in this field before you can save a Work Pack. |
Work Pack Description |
Character |
A description of the Work Pack |
This is a required field. You must enter a value in this field before you can save a Work Pack. |
Pipe Rotation Event
Pipe Rotation Event family is used in Thickness Monitoring module to capture Rotation or Flip movements for Piping Assets. The following table provides an alphabetical list and description of the fields that exist in the Piping Rotation Event family.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Component ID | Character | Specifies a unique ID for the component that is rotated or flipped. | This field is automatically populated during a rotation or flip. This field is always disabled. |
Movement Date | Date | Stores the date of the rotation or flip. | This field is automatically populated during a rotation or flip. This field is always disabled. |
Moved By | Character | Stores the Security User key of the user that performed a rotation or flip. | This field is automatically populated during a rotation or flip. This field is always disabled. |
Move Type | Character | Identifies the type of movement that occurred. For example, Rotate or Flip. | This field is automatically populated during a rotation or flip. This field is always disabled. This field is populated by the MI_PIPE_MOVE_TYPES System Code Table. |
Rate Method | Character | Stores the Rate Method specified when performing a rotation or flip. | The value in this field must be selected when performing a rotation or flip. |
Remaining Life Before | Numeric | Stores the remaining life of the component, prior to the rotation or flip. | This field is automatically populated during a rotation or flip. This field is always disabled. |
Retirement Date Before | Date | Stores the retirement date of the component, prior to the rotation or flip. | This field is automatically populated during a rotation or flip. This field is always disabled. |
Remaining Life After | Numeric | Stores the remaining life of the component after the rotation or flip. | This field is automatically populated during a rotation or flip. This field is always disabled. |
Reverted | Boolean | Identifies Pipe Rotation Events that have been reverted. | This field is automatically set to True when a Pipe Rotation Event undo an action. This field is always disabled. |
Rotation Sequence Number | Numeric | Stores the sequence number of the rotation of the component. | This field is automatically populated during a rotation or flip. This field is always disabled. |
Scenario ID | Character | Stores the Scenario ID for a What If scenario. | The value in this field must be entered when a What If scenario is created. |
Top Center Moved To | Numeric | Stores the Position ID of the position that the Top-Center position was moved to. | This field is automatically populated during a rotation or flip. This field is always disabled. |
What If Method | Character | Stores the method used to generate the What If scenario. |
This field is populated automatically when a What If scenario is created. This field is populated by the MI_PIPE_WHAT_IF_TYPES System Code Table. This field is always disabled. |