Calibration Planning
Calibration Management: Calibration Planning Workflow
This workflow describes the planning process involved in conducting calibration, including setting up the required tools (i.e., test equipment, standards, engineering design information), defining the strategy, and scheduling the calibration.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram. For more information, refer to the topic Interpreting the Workflow Diagrams.

Define Test Equipment and Standards
Persona: Analyst
Identify the tools (i.e., Test Equipment such as documenting process calibrators and Standard Gas Cylinders) needed to perform the calibration. Standard Gas Cylinders are used to calibrate single component and multi-component analyzers. Gather the necessary engineering design information for an asset that you want to calibrate. This is required to develop a calibration strategy, and to ensure that you adhere to regulatory compliance.
Define Calibration Defaults
Persona: Analyst
Define the error limits and the type of error assessment to be used for each type of calibration. These details are stored in a Calibration Setup Defaults record.
Select Profile Template
Persona: Analyst
Select a Profile Template for a specific type of calibration.
Administration
Persona: Analyst
Select the strategy for the template type to specify the strategy that will be used in a Calibration Profile.
Go to the Calibration Administration workflow.
Select Calibration Strategy
Persona: Analyst
Select the strategy for the template type to specify the strategy that will be used in a Calibration Profile.
Go to the Calibration Administration Workflow.
Create Calibration Profile
Persona: Analyst
Create a Calibration Profile to group all the Assets that you want to calibrate using a single template. Provide a unique name for the profile, and link a Profile Template.
Link Assets to Profile Template
Persona: Analyst
Link the Calibration Profile to Assets that you want to calibrate using a single template. For each Asset that you have linked to the profile, GE Digital APM creates a copy of the template. The Asset and the template (copy) combination is called the Applied Profile. If needed, you can modify the asset-related information in the applied profile.
Asset Strategy Management (ASM)
Persona: Analyst
GE Digital APM Asset Strategy Management (ASM) software module. The ASM module is available in GE Digital APM and the appropriate license of ASM is required.
Go to the Asset Strategy Management Workflow.
Enterprise Asset Management (EAM)
Persona: Analyst
Enterprise Asset Management (EAM) software (i.e., SAP, Maximo). The EAM software is a third-party software and not a part of GE Digital APM.
Go to the EAM Work Management: Work Order Generation Workflow.
Create Calibration Task
Persona: Analyst
Create a Calibration Task to specify the schedule for performing the calibration and to assign the task to a user. This Calibration Task is linked to the Asset and the Template combination (called the Applied Profile). The Calibration Task is listed in the Calibration Queue section of the Calibration Management Overview page.
Perform Calibration Assessment
Persona: Analyst
Go to the Calibration Assessment Workflow.