GridOS® WAMS

GridOS® WAMS

Precisely monitor
grid oscillations

GridOS Wide Area Monitoring System (WAMS) empowers grid operators to verify normal oscillation behaviors. Its robust analysis engine can quickly identify and pinpoint the precise cause of any disturbance, enabling operators to intervene before outages occur. 

GridOS® WAMS

Overview

Maximize grid stability across transmission 

Transmission operators face a variety of challenges associated with the energy transition. Increased renewables integration, reduced inertia, more sensitive voltage profiles, and an overall growing demand for electricity create complexities that must be resolved before disruptions result. 

The advanced monitoring and analysis capabilities of WAMS enable transmission operators to understand real-time grid dynamics and take proactive action to maintain and restore system stability. 
WAMS - A powerful WAMS solution built for grid orchestration

A powerful WAMS solution built for grid orchestration

GridOS WAMS offers applications such as Oscillation Monitoring and Source Location, Disturbance Detection, Islanding Re-Synchronization Support, Effective Inertia Metering, and Dynamic Model Validation & Calibration – all of which help transmission operators proactively orchestrate the grid.

    Better technology.
    Fewer outages. 

    With GridOS WAMS’ robust analysis capabilities, operators can monitor grid oscillations and verify normal activity. With Oscillation Source Location, operators can locate generator units that are destabilizing the grid and take corrective actions to prevent outages. In cases where electrical islands have formed, GridOS WAMS can help operators understand if those islands are electrically balanced, guaranteeing a smooth reconnection during the re-synchronization phase. 

    It all adds up to better system awareness, leading in turn to improved grid stability and fewer outage situations. 

    Gartner® states, "PMUs boost situational awareness, detecting congestion and grid oscillations. WAMS, with embedded AI and event handling, swiftly pinpoints root causes and recommends actions — based on multiple phasor measures per second — to operators and traders."

    Gartner, Hype Cycle™ for Digital Grid 2024, Lloyd Jones, Jo-Ann Clynch , 8 July 2024

    GARTNER is a registered trademark and service mark of Gartner, Inc. and/or its affiliates in the U.S. and internationally, and HYPE CYCLE is a registered trademark of Gartner, Inc. and/or its affiliates and are used herein with permission. All rights reserved.

    Explore the benefits of GridOS WAMS

    WAMS - Faster Disturbance Analysis

    Faster Disturbance Analysis

    Leveraging GridOS WAMS, system operators have decreased the disturbance analysis process from days to hours. 

    WAMS - Fewer Blackouts

    Fewer Blackouts

    GridOS WAMS can proactively identify and locate oscillation sources in real time, helping operators take corrective action before grid blackouts can occur.

    WAMS - Maximum Visibility

    Maximum Visibility

    GridOS WAMS provides the clearest, fullest view of the transmission network, including imminent disturbances and their root causes. 

    WAMS - Better Stability

    Better Stability

    GridOS WAMS includes a full automated frequency-control tool - essential for grids with high integration of renewables. 

    WAMS - Simpler Compliance

    Simpler Compliance

    GridOS WAMS fully meets NERC requirements for grid dynamics and offers a non-intrusive tool to verify NERC generator compliance.

    WAMS - Seamless Scalability

    Seamless Scalability

    Start small, or roll out at scale. Thanks to the GridOS microservice-based architecture, GridOS WAMS can be scaled to match any size operation.

    Resources

    Videos

    FAQs

    FAQs

    What is Wide Area Monitoring System (WAMS)?
    A Wide Area Monitoring System (WAMS) is an advanced transmission power grid software solution to enhance the monitoring and control of large-scale transmission networks. WAMS provides real-time data and situational awareness over wide geographical areas, which is critical for maintaining grid stability and grid reliability.

    What is WAMS used for?
    WAMS, or Wide Area Monitoring Systems, are primarily used in the context of electrical power systems. These systems leverage advanced measurement technologies, such as Phasor Measurement Units (PMUs), to provide real-time monitoring and analysis of electrical grid operations over large geographical areas. The primary uses of WAMS include:

    • Grid Stability and Reliability: WAMS monitors the stability and dynamic performance of the power grid, enabling operators to detect and address system disturbances or anomalies promptly.
    • Situational Awareness: By providing real-time data, WAMS enhances situational awareness for grid operators so they can make informed decisions and improve operational efficiency.
    • Early Warning and Alerts: WAMS can provide early warnings of potential issues, such as oscillations, helping prevent blackouts and improving system reliability.
    • Optimization and Control: WAMS can be used to optimize grid operations and improve control strategies by providing accurate and timely information about grid conditions.
    What are the benefits of Wide Area Monitoring System (WAMS)?
    A WAMS offers several benefits that increase the efficiency, reliability, and security of electrical power systems.

    Key benefits of WAMS:

    • Real-time Data Acquisition: WAMS uses Phasor Measurement Units (PMUs) to collect real-time data on voltage, current, frequency, and phase angle across the grid. This data is essential for understanding the dynamic behavior of the transmission power grid.
    • Enhanced Situational Awareness: By providing a comprehensive view of grid operations over a large area, WAMS helps operators detect and respond to disturbances and anomalies quickly, preventing potential outages or grid failures.
    • Grid Stability and Reliability: WAMS contributes to grid stability by enabling operators to monitor and manage power flows, detect oscillations, and address potential stability issues proactively.
    • Support for Renewable Integration: WAMS facilitates the integration of renewable energy sources by providing the necessary data to manage their variability and ensure their efficient use within the grid.
    • Advanced Analytics and Decision Support: The system leverages advanced analytics to provide insights and decision support, helping operators make informed decisions to optimize grid performance.
    • Coordination Across Regions: WAMS enables better coordination and collaboration between different regions and grid operators, enhancing the overall efficiency and reliability of interconnected power systems. This is especially valuable for synchronous electrical grids, like Europe’s Continental Synchronous Area.

    GridOS WAMS is a critical component in modernizing the transmission power grid, providing the tools and data needed to manage increasingly complex and dynamic electrical systems.

    How does WAMS empower a smart grid?
    WAMS is a key component of a smart grid with its enhanced monitoring, control, and optimization capabilities. Here is how WAMS contributes to the development and operation of smart transmission grids :

    • Real-time Data Collection: WAMS utilizes Phasor Measurement Units (PMUs) to gather real-time data on voltage, current, frequency, and phase angles across the grid. This data is crucial for the smart grid's ability to monitor and manage grid conditions dynamically.
    • Improved Situational Awareness: By offering a comprehensive, wide-area perspective of grid operations, WAMS enhances situational awareness for operators. This capability is essential for the smart grid's goal of maintaining reliability and stability under varying conditions.
    • Enhanced Grid Stability: Smart grids aim to be more resilient and adaptive. WAMS supports this by providing the tools to detect and mitigate stability issues, such as oscillations, that can arise from complex grid interactions.
    • Integration with Renewable Energy Sources: Smart grids are designed to support the integration of renewable energy. WAMS facilitates this by providing the necessary data and analytics to manage the variability and distributed nature of renewables effectively.
    • Grid Optimization and Efficiency: Through real-time monitoring and data analytics, WAMS contributes to optimizing grid operations, reducing energy losses, and enhancing overall efficiency, which are key goals of the smart grid.
    • Interoperability and Coordination: WAMS enables better coordination across different grid regions and systems, fostering interoperability—a core principle of smart grid development. This capability supports seamless communication and collaboration between various grid components.

    What is WAMS in smart grid?
    Wide Area Monitoring Systems (WAMS) play a significant role in enhancing the functionality and reliability of smart grids. Here are some key roles that WAMS fulfill in smart grid environments:

    Real-Time Monitoring: WAMS provide real-time monitoring of grid conditions over large geographic areas, enabling operators to detect and respond to disturbances quickly. This real-time data helps in maintaining grid stability and reliability.

    Data Collection and Analysis: WAMS collect detailed data on various grid parameters, such as voltage, current, and frequency, using Phasor Measurement Units (PMUs). This data is crucial for analyzing grid performance and identifying trends or anomalies.

    Improved Situational Awareness: By offering comprehensive visibility into grid operations, WAMS enhance situational awareness for grid operators. This awareness is vital for effective decision-making and timely interventions during grid disturbances.

    Grid Stability and Control: WAMS help in monitoring and controlling grid stability by providing insights into dynamic grid behavior. This capability is essential for managing power flow and preventing cascading failures during disturbances.

    Support for Renewable Integration: WAMS facilitate the integration of renewable energy sources by providing real-time data that helps manage their variability and intermittency. This ensures that renewables are effectively integrated into the grid without compromising stability.

    Fault Detection and Management: WAMS can detect faults and disturbances in the grid, enabling rapid identification and isolation of problem areas. This helps minimize the impact of faults and improve service reliability.

    Enhanced Grid Security: By providing detailed insights into grid operations, WAMS contribute to grid security by enabling early detection of potential threats or anomalies that could compromise grid integrity.

    Optimization of Grid Operations: The data and insights provided by WAMS support the optimization of grid operations, including load forecasting, demand response, and network optimization, leading to more efficient and reliable grid performance.

    Overall, WAMS are integral to the development and operation of smart grids, providing the advanced monitoring and analytical capabilities necessary to manage modern, complex power systems effectively. They enable utilities to enhance grid performance, integrate diverse energy sources, and ensure reliable service delivery in a dynamic energy environment.
    Customer Stories

    Customer Stories

    Speak with a utility software expert about how GridOS can help ensure a reliable and resilient sustainable-energy grid.

    Fill out the form below or call us at 1-833-690-5552.

    Thank you for getting in touch! 

    We’ve received your message, One of our colleagues will get back to you soon. Have a great day!