As the share of renewables in the electricity mix continues to grow, network operators are looking at ways to integrate them into the distribution network more efficiently.
UK Power Networks is partnering with GE Vernova on a world-first smart substation project designed to optimize utilization of the distribution network to facilitate the rise of renewable energy generation across the United Kingdom.
Known as
Constellation, the project aims to release 1.4 GW of capacity (enough to power more than 700,000 homes) and save consumers more than £750 million by 2050. It is also forecast to save more than 17.8M tons of harmful greenhouse gas emissions by 2050.
Smart substations optimize distribution network utilization and contribute to net-zero targetsConstellation is a world-first innovation project that will see powerful computers installed in a series of substations, turning them into smart substations. It provides a unique approach to distribution network management through decentralized operation using data analytics and machine learning, reducing reliance on communications to and from the central control systems
A key aspect of Constellation is the installation of GE Vernova’s
PhasorController in substations to enable the deployment of multiple smart applications. This will include functionality to optimize distribution network utilization and contribute to net-zero targets while reducing the need for investment in additional infrastructure.