GridOS® DERMSNext-Level DER OrchestrationMillions of distributed energy resources (DERs) are added to the grid every year. Harnessing their full potential requires a modern, integrated power system with real-time, advanced orchestration capabilities. Look no further than GridOS DERMS, GE Vernova’s #1-ranked DER management system.Learn about DERMS' role in the energy transition GridOS® DERMS Overview Simplify DER complexity As DER integration grows, so do the complexities it introduces. GridOS DERMS addresses these challenges head-on with industry-leading DER orchestration capabilities that simplify electrical complexities, unlock techno-economic optimization, and proactively resolve grid violations. GridOS DERMS is the must-have DER solution for the modern utility. Named the #1 Grid DERMS provider by Guidehouse InsightsGridOS DERMS is expertly designed to efficiently orchestrate the rapidly increasing integration of DERs. Its suite of advanced, modular applications covers the full DER management lifecycle—from initial integration and visualization to ongoing operation, control, and optimization.Download Report A powerful DERMS for the modern utility 90+More than 90 deployments globally 127MServing 127 million utility service points #1Ranked #1 in Grid DERMS by Guidehouse Insights Optimizing the grid with GridOS DERMS Increased grid reliability GridOS DERMS unlocks the full value of DERs, optimizing power flow and enhancing grid reliability. Enhanced situational awarenessGet the clearest real-time (and look-ahead!) view of all connected DERs and their impact on the grid. Streamlined T&D coordinationGridOS DERMS seamlessly integrates with ADMS, AEMS, Edge DERMS, and Markets, offering unified management for full visibility, coordination, and control across T&D. Easier compliance with standards and regulations GridOS DERMS adheres to numerous industry standards like OpenADR and IEEE 2030.5, with the flexibility and scalability to adapt to new or changing regulations into the future. Proactive operationsLeverage GridOS DERMS’ precise look-ahead analysis to anticipate backfeeds, predict power shortfalls or surpluses, and more to unlock proactive grid orchestration. Scalability and future readiness Start small and expand over time, or roll out at scale. GridOS DERMS scales with any size operation, with the flexibility to adapt to changing needs over time. Load More As noted by Gartner®, "The operational impacts of high DER capacity, particularly when it reaches significant thresholds like 15% of peak load, underscore the necessity of DERMS for maintaining grid stability and reliability."Gartner, Hype Cycle™ for Power and Utility Industry IT, 2024, Nicole Foust – 3 July 2024GARTNER is a registered trademark and service mark of Gartner, Inc. and/or its affiliates in the U.S. and internationally, and HYPE CYCLE is a registered trademark of Gartner, Inc. and/or its affiliates and are used herein with permission. All rights reserved. Advanced capabilities, simplified for grid operators As grids grow more complex and interconnected, GridOS DERMS ensures operators have the tools they need for real-time, modular control. With capabilities designed to adapt to both present and future grid challenges, GridOS DERMS is not just a solution today but a framework for the grid of tomorrow.GridOS DERMS is not a one-size-fits-all solution. Its modular design ensures the solution can adapt to and scale with the diverse and evolving needs of utilities. The core modules of GridOS DERMS consist of: Model Manager: Maintains and ingests network and DER asset data, ensuring accurate and up-to-date information.Program Manager: Serves as a single source of truth for program, contract, and enrollment data, while providing robust reporting on program performance and constraints.Gateway: Acts as a single point of communication for monitoring and control between DERs and aggregators, certified to IEEE 2030.5 standards.Operations: Offers situational awareness through a unified interface, enabling the visualization of alerts and efficient management of grid operational issues. Forecasting: Continuously predicts load and generation using an extensive library of models, enhancing grid reliability.Optimization: Provides optimal scheduling of DERs based on grid constraints, economics, and dynamic operating envelopes.Markets Orchestration: Supports intelligent decision-making for techno-economic optimization, enhancing market participation.Flex Planning: Facilitates short-term operational planning and long-term scenario planning, including non-wires alternatives optimization, with study mode capabilities. Additional Resources Unlock Grid Capacity with Flexible InterconnectionsLearn how GridOS® DERMS enables flexible interconnections to unlock greater grid capacity.Download Solution Paper Prepare for DER FlexibilityLearn how GridOS DERMS enable markets at scale!Download Solution Paper DER management at StedinLearn how GE Vernova helped Dutch DSO Stedin orchestrate its DERs.Watch webinar Load More View All Resources Resources Blogs Videos Additional Resources FAQs FAQs What is a Distributed Energy Resource? A Distributed Energy Resource (DER) is a small-scale unit of electricity generation or storage that is connected to a larger power grid at the distribution level. DERs are typically renewable energy sources such as solar PV systems, electric vehicles (EVs), or energy storage, that play a crucial role in modernizing the grid by providing flexibility, enhancing grid resilience, and enabling the integration of renewable energy sources. What is a Distributed Energy Resource Management System? A Distributed Energy Resource Management System (DERMS) is a software platform designed to manage and optimize the operation of Distributed Energy Resources (DERs) within an electric grid. DERMS enables grid operators to monitor, control, and coordinate a variety of DERs such as solar panels, battery storage, smart thermostats, and more. How do DERMS work? DERMS solutions leverage advanced algorithms and real-time data analytics to determine how DERs are behaving, plus their current and future impacts on the grid. The insights they provide make it faster and easier for utilities businesses to integrate and manage DERs within the electrical grid, leading to better grid reliability, efficiency, and sustainability. What are the benefits of DERMS on the grid? With the right DERMS in-house, utilities can increase grid reliability and resilience, improve energy efficiency, effectively integrate renewable energy sources, avoid backfeeds, and unlock techno-economic optimization for better markets participation, among other benefits. By providing real-time data and analytics capabilities, a DERMS helps optimize DER performance and supports their integration into the broader grid. What is a Grid DERMS? A Grid DERMS is a centralized DERMS solution designed to manage and optimize DERs to achieve grid-level outcomes. These outcomes include enhanced grid reliability and resilience, improved energy efficiency, and the seamless integration of renewable energy sources.A Grid DERMS connects and integrates various DERs—such as solar PV systems, energy storage, and electric vehicles (EVs)—into the power grid. It collects data from these resources, analyzes grid-wide conditions, and executes optimized control actions to align with the grid’s operational objectives. This centralized approach provides utilities and grid operators with a holistic view of the entire grid, enabling improved planning, coordination, and optimization. What is the Difference Between Grid DERMS and Edge DERMS? The key difference between Grid DERMS and Edge DERMS lies in their management and control strategies. Grid DERMS operates as a centralized system, managing DERs from a unified platform to optimize grid-wide performance and ensure system-level control. On the other hand, Edge DERMS focuses on enabling DER and demand response services by engaging directly with DER owners and end customers, offering aggregation services and localized control.Coordination between Grid DERMS and Edge DERMS allows grid operators to achieve enhanced grid performance through improved situational awareness, adapt to various grid configurations, and empower DER owners and customers to actively participate in energy management. Together, these solutions create a dynamic and collaborative framework that supports the evolving needs of the energy transition. What are the challenges of distributed energy resources? DERs are crucial for modernizing and stabilizing the energy grid, but they also present several challenges that need to be addressed—including cybersecurity, regulatory complexity, and integration difficulties—to ensure effective integration and operation.Key challenges of DER include:1. Grid Integration: Integrating thousands of new DERs into existing grid infrastructure can be complex, requiring advanced control systems and protocols to ensure seamless operation and communication between diverse energy sources.2. Intermittency: Many DERs, such as solar and wind, are dependent on weather conditions – simply because the sun isn’t always shining and the wind isn’t always blowing. This leads to inconsistent energy production, requiring robust forecasting and energy management software to maintain grid stability.3. Regulatory and Policy Barriers: Varying regulations and policies across different regions can hinder the deployment and operation of DERs, necessitating advanced DERMS software to support their growth and maintain compliance.4. Cybersecurity Risks: As DERs become increasingly digitized and interconnected, the utilities that oversee them become increasingly vulnerable to cyber threats. Ensuring cybersecurity is crucial to protect sensitive data and maintain operational integrity. A built-in Zero Trust grid security model is one way of providing an optimal level of cybersecurity.5. Capacity and Reliability: Managing the capacity and reliable performance of DERs, especially in high-demand scenarios, can be difficult and requires sophisticated energy management systems and infrastructure upgrades.Addressing these challenges involves coordinated efforts across technology investments, policymaking, and industry collaboration to unlock the full potential of DERs in driving reliability and resilience in the sustainable energy future. What is an example of a DER? Some of the most common examples of DERs include solar PV systems, wind turbines, EVs, and storage batteries. What are the benefits of DER? Distributed Energy Resources (DERs) offer numerous benefits, contributing to the efficiency, reliability, and sustainability of energy systems. Here are some of the key advantages:Enhanced Grid Resilience: DERs can improve grid resilience by diversifying energy sources and reducing reliance on centralized power generation. In the event of grid disruptions, DERs can provide local power support, especially when organized as a microgrid.Increased Energy Efficiency: By generating energy closer to where it is consumed, DERs reduce transmission and distribution losses, leading to more efficient energy use.Reduced Environmental Impact: Many DERs, such as solar panels and wind turbines, are renewable and produce electricity without emitting greenhouse gases, thus helping to lower the carbon footprint of energy systems.Cost Savings: DERs can lower energy costs for consumers by providing alternatives to traditional power sources and reducing demand on the grid, particularly during peak periods.Energy Independence: DERs can enhance energy independence for individuals and communities by enabling them to produce their own power, reducing reliance on external suppliers.Grid Flexibility and Stability: DERs contribute to grid flexibility by providing additional sources of generation and storage, which can be dispatched as needed to balance supply and demand.Support for Renewable Integration: DERs facilitate the integration of renewable energy into the grid, providing complementary resources that can be adjusted based on availability and demand.Economic Opportunities: The deployment of DERs can stimulate economic growth by creating jobs in manufacturing, installation, and maintenance of these systems.Scalability: DERs can be scaled according to specific needs, allowing for tailored solutions that meet the energy demands of different users and regions.Improved Reliability: With multiple generation sources, DERs can improve the reliability of power supply, reducing the risk of outages.Overall, DERs play a crucial role in modernizing energy systems, promoting sustainability, and enhancing grid performance. Their adoption can lead to more resilient, efficient, and environmentally friendly energy solutions. Partners DER management: A true team sportGridOS DERMS is paving the way towards optimal, complete DER orchestration through its dynamic and expanding partner ecosystem. Each partner contributes DERMS-specific technology or cloud and system integration capabilities to help unlock new data streams, improve visibility, expedite deployment, and overall maximize value for GridOS DERMS users. Our partners include: EnergyHubGridOS DERMS users can better monitor and optimize edge DERs with EnergyHub’s Edge DERMS tools and data. NodesWith GridOS DERMS and NODESmarket platform, utilities can better access and acquire grid flexibility when needed. EPEX SpotThe EPEX SPOT partnership expedites renewables integration and minimizes congestion through flexibility access. PicloPiclo’s grid flexibility platform integrates readily with GridOS DERMS, ensuring better resilience. Clean Power ResearchClean Power Research’s PowerClerk solution and GE Vernova’s GridOS applications share data for better grid insights. WeaveGridWeaveGrid provides invaluable insights on EVs and their impact on the grid. PlexigridPlexigrid's software augments GridOS DERMS with LV grid monitoring, planning, and simulation capabilities. Load More Get in TouchGet in Touch Connect with a utility software expert about how GridOS can help ensure a reliable and resilient sustainable-energy grid.Fill out the form below. Thank you for getting in touch! We’ve received your message, One of our colleagues will get back to you soon. Have a great day!