Logon Scripts
About this task
Logon scripts allow administrators to configure the operating environment for Webspace users. Scripts may perform an arbitrary set of tasks such as defining user-specific environment variables and drive letter mappings.
Webspace supports two types of logon scripts: global scripts that execute for all users that log on to the server, and user-specific scripts that execute for individual users. Before loading the user's profile, Webspace checks to see if a script of either (or both) type has been specified. If so, Webspace runs the script(s) within the user's security context each time the user is authenticated.
User-specific logon scripts are specified using the functionality provided by the operating system. For example, the logon script for local users on a Windows 2000 server is specified as follows:
- Right-click My Computer and click Manage.
- Navigate to the \System Tools\Local Users and Groups\Users folder.
- Select a user and click Properties.
- Click Profiles.
- In the Logon script box, type the file name of the user's logon script.
If the value entered in the Logon script box specifies a file name and extension only, Webspace searches for the file in the following directories, in the following order:
- If the user's account is a domain account is the NETLOGON share of the primary domain controller (for example: \\pdcname\NETLOGON), or the domain subdirectory of the primary domain controller's SYSVOL share (for example: \\pdcname\SYSVOL\domainname).
- If the user's account is a local account. For example: systemroot\System32\Repl\Import\Scripts or systemroot\sysvol\sysvol\domainname.
If the logon script is stored in a subdirectory of one of the above directories, precede the file name with the relative path of that subdirectory. For example: Admins\JohnG.bat.
Administrators specify global and user-specific logon scripts through the Webspace Admin Console's Session Startup dialog.
Running User-specific Logon Scripts
Procedure
- From the Webspace Admin Console, in the server tree, select the desired server from the list.
- On the Tools menu, click Host Options. The Host Options dialog box appears.
- Click the Session Startup tab.
- Select the User-specific check box.
- Click OK.
Running a Global Logon Script
Procedure
- From the Webspace Admin Console, in the server tree, select the desired server from the list.
- On the Tools menu, click Host Options. The Host Options dialog box appears.
- Click the Session Startup tab.
- Select the Global check box.
-
In the field next
to the check box, specify the path of the global script file.
For example, you may want to add the LoginScript.bat, provided in the C:\Program Files\Proficy\Webspace Server\Programs folder as an example for configuring mapped drives, as a global script.
-
Click OK.
Note:Authenticated users must have read and execute access to the logon script files. An example of a logon script is described in the Creating Mapped Drives on the Webspace Server section. The LoginScript.bat example described in this section can be applied on a global or user-specific basis.