Connections based on URLs
You define which URLs a browser can use to connect to Web HMI. This is particularly useful for mobile devices without access to DNS lookups.
You defined the list of acceptable URLs in the Host Name fields on the Configure Host and Port screen during installation. For example, if w2012r2 was entered as a host name, Web HMI will accept a connection request from https://w2012r2/WebHMI/login.html. The host values, which can also be IP addresses, are stored in the Reverse Proxy configuration file (default location: C:\Program Files\Proficy\ProficyWebServer\ReverseProxy\serverConfig.json). You can update this list in the host name field of the serverConfig.json file.