About UAA Users
The user is an individual with privileges for your Proficy application.
You can create users locally in UAA for authentication and assign them to the required groups from the UAA Configuration Tool.
Users can added to Proficy UAA in two ways:
- Directly adding users: You can create a new user using the UAA Configuration Tool, or using any UI provided by a product which uses Proficy UAA.
- Mapping existing user groups: If you have user groups in an existing UAA instance, LDAP service, or SAML service, you can map these groups with the Proficy UAA group. The users of these groups can then use Proficy UAA.
You can directly add users to Proficy UAA by accessing the Users section of the UAA Configuration Tool.