Add Server Nodes for Validation

This topic describes how to select computers during validating a cluster configuration.

About this task

In the following steps, UAAHANODE1 (Node1 server name) and UAAHANODE2 (Node2 server name) are used as example server nodes in a cluster.

Procedure

  1. On the Select Servers or a Cluster tab, select Browse.
    The Select Computers screen appears.
  2. Select Advanced.
  3. Select Find Now.
    A screen appears prompting to enter the network credentials.
  4. Enter the user name and password of the domain where the cluster validation is being performed, and select OK.
    After successful login, you can see the associated nodes.
  5. Select UAAHANODE1 and UAAHANODE2, and select OK.
  6. Select OK to exit.