System Requirements for Modules
APM Connect System Requirements
License Requirements
APM Connect has a two-tier license system that enables the APM Connect Framework. One of the following license types is required to take advantage of the APM Connect functionality:
- APM Connect Basic
- APM Connect Plus
Additional Licensing
The following additional licenses are required to take advantage of the SAP Adapters:
- SAP Integration Interfaces:
- Enables the SAP Equipment, Functional Location, Work History, and Notification Creation Adapters.
- SAP Technical Characteristics:
- Enables the SAP Technical Characteristics Adapter.
- SAP Work Management:
- Enables the SAP Work Management Adapter.
The following additional license is required to take advantage of the SAP PI Adapters:
- SAP Process Integration:
- Enables the SAP PI Adapters.
The following additional license is required to take advantage of the Maximo Adapters:
- Maximo Interfaces:
- Enables the Maximo Equipment, Functional Location, Work History, Service Request, and Work Order Generation Adapters.
The following additional license is required to take advantage of the ServiceMax Adapters:
- ServiceMax Enterprise License:
- Enables ServiceMax Installed Product and Service Request Generation Adapters.
UDLP Versions
Beginning with the Sept. 21, 2018 release, Predix Essentials will maintain compatibility with the APM Connect client-side jobs one version prior to the newly released version.
To prevent processing failures, you must upgrade your on-premises, client-side jobs within two months of a Predix Essentials release to the most current version of the APM Connect client jobs. For example, if the Predix Essentials tenant has installed the Dec. 14, 2018 release, you must upgrade the on-premises, client-side jobs to UDLP V2.5.0 or V2.5.1 by Feb. 14, 2019, otherwise the next release of the Predix Essentials tenant may not process your data correctly.
The following UDLP versions are currently supported in Predix Essentials:
- V2.9.0
Recommended Software for APM Connect Server
- Windows Server 2016 R2
Browser Requirements for APM Connect Server
Web Browser | Recommended or Supported |
---|---|
Google Chrome | Recommended |
Microsoft Internet Explorer 10 | Supported |
Microsoft Internet Explorer 11 | Supported |
Minimum Hardware Requirements for APM Connect Server
- Four Processor Core, 2.0GHz
- 16 GB RAM
- 100 GB Free Disk
- 100 MB Network Interface
Recommended Hardware for APM Connect Server
- I5 Processor, 2.0 + GHz
- 32 GB RAM
- 300 GB Free Disk
- 1 GB Network Interface
Depending on how your system is configured, these requirements may not be sufficient. Parameters that affect the hardware requirements include the number of users, modules purchased, database size, and other factors that can vary from one customer to another. For help refining your specific system requirements, contact GE Digital
APM Foundation System Requirements
License Requirements
This feature is available with the core Predix Essentials application; no specific license is required.
Asset Criticality Analysis (ACA) System Requirements
License Requirements
This feature is available in the Predix Essentials application with the Meridium Core license; no specific license is required.
ACA integration with SAP is only available in on-premises releases.
To update your SAP system to reflect the criticality value that is determined in ACA, the licenses SAP Interfaces – Foundation and SAP Interfaces - Criticality Assessment are also required.
Additional Components Required
Only the basic Predix Essentials system architecture is required for this feature to work correctly. No additional components are required.
Family Policy System Requirements
License Requirements
The Family Policy license is required to take full advantage of Family Policy functionality.
Additional Components Required
Only the basic Predix Essentials system architecture is required for this feature to work correctly. No additional components are required.
Metrics and Scorecards System Requirements
License Requirements
The Metrics Manager license is required to use the Metrics and Scorecards module.
Additional Components Required
In addition to the basic Predix Essentials system architecture, your system must also contain the following additional components:
-
A SQL Server Analysis Services Server machine that will host the Microsoft SQL Server Analysis Services software. The following versions of SQL Server Analysis Services are supported in this version of Predix Essentials:
- Microsoft SQL Server Analysis Services 2014
- Microsoft SQL Server Analysis Services 2016
-
If you are using an Oracle database, to process the Work History cube, you must install ODP.NET (Oracle Data Provider.NET), an Oracle Data Access Component, on the machine where the Work History cube is deployed.
Policy Designer System Requirements
License Requirements
The Policy Designer license is required to take full advantage of Policy Designer functionality.
This license is not required for the module workflow policies to operate; however, if you want to modify a module workflow policy, the Policy Designer license is required. You do not need the Policy Designer license to view module workflow policies for modules for which you have a license.
Recommendation Management System Requirements
License Requirements
The Meridium Core license is required to take advantage of the Recommendation Management functionality.
Reference Documents System Requirements
License Requirements
This feature is available with the core Predix Essentials application; no specific license is required.