Admin
Access the Policy Admin Page
About This Task
Procedure

Configure Execution History Retention Settings
About This Task
You can configure the execution history retention settings to specify the time for which execution history records for policies must be retained in the Predix Essentials database. You can configure the settings to retain the execution history records for executions that result in Errors, Warnings (Action Taken), Warnings (No Action Taken), Success (Action Taken), or Success (No Action Taken), either for an indefinite period or for a specific duration. By default, the execution history records are configured to be retained for an indefinite period. If you configure the settings to retain these records for a specific duration, an automated job deletes the records that have been retained in the database for more than the specified duration. You can specify the interval at which the job must run.
- The Policy execution log can grow quickly and significantly impact the size of the Predix Essentials database. You can control the size of the execution log by minimizing the time that the execution history is retained in the Predix Essentials system and also by selecting an appropriate execution history setting for each policy.
- The execution history retention settings are not specific to a policy and are applicable for all policies. The settings are also applicable to any execution history records for the Family Policies.
- The most recent execution history of each instance associated with a policy is retained in the database even if it exceeds the specified retention duration.
- Depending on the number of old execution history records that exists when the retention settings are configured, it may take multiple runs of the automated job to delete all the old execution history records.
This topic describes how to configure the settings to retain the execution history records for policies for a specific duration in the database depending on the execution result.