Policy Management
About Family Policies
You can use family policies to configure certain actions to occur when a record changes in the Predix Essentials database. For example, you can specify that after a Reading record is added to the database, it should be linked to a Measurement Location record.
When you create a family policy, you will configure a policy model to represent the inputs, logic, and actions that you want to execute when the corresponding trigger occurs. You can create up to six family policies for a single family, one for each supported type of trigger.
Policy Model

- The items that you want to monitor (for example, Reading in Error records).
- The conditions that should trigger actions to be taken (for example, a comment is something other than test).
- The actions that should be taken (for example, send an email message).
A policy model does not function like a typical logic diagram. For example, a node does not automatically evaluate the values from the immediately preceding node. Rather, for each node, you can specify an input value that is associated with any predecessor node, even if the nodes are not directly connected. Before you create a policy model, make sure that you understand the basic principles for working with a policy model.
Family Policy Triggers
For any family, you can create one family policy for each available trigger. Predix Essentials supports the following triggers for family policies.
Trigger | Description |
---|---|
Before Insert | Executes the policy before a record is created. |
After Insert | Executes the policy after a record is created. |
Before Update | Executes the policy after changes have been made to a record, before those changes are saved to the database. |
After Update | Executes the policy after changes to a record have been saved. |
Before Delete | Executes the policy before a record is deleted. |
After Delete | Executes the policy after a record has been deleted. |
Create a Family Policy
Procedure
Access a Family Policy
Procedure
Refresh Metadata for Family Policies
About This Task
Procedure
- Access the policy for which you want to refresh the metadata.
- In the Design workspace, perform one of the following steps:
- If you want to refresh the metadata for the policy, in the Edit section of the toolbar, select
.
The metadata for the policy is refreshed.
- If you want to refresh the metadata for a node, select the node, and then in the Properties window for the node, select
.
The metadata for the node is refreshed.
- If you want to refresh the metadata for the policy, in the Edit section of the toolbar, select