Email Settings Configuration
Configure Email Settings
Procedure
- Access the Email Settings page.
- In the From box, enter the email address that you want to appear in the From field of emails generated by Predix Essentials.Note:
- By default, the notification emails are sent from [email protected].
- Email address is case sensitive. For example, if you verify [email protected], you cannot send email from [email protected] unless you verify [email protected] as well.
A warning message appears, asking you to verify the email address.Important: If the email address is not verified, the email notifications will not be sent. - Select Verify Email.The verification email is sent from [email protected] to the email address configured in the From boxNote: If the email address is already verified, further steps are not required.
- Access the email inbox that you configured in the From box.
- Click on the verification link received in the email from [email protected] to complete the email verification process.
- Select
.
All the emails are now configured to be sent via Amazon SES .Tip: To send a test email to confirm that email settings have been configured successfully, select Test Settings, then, on the window that appears, enter values in the available fields, and then select Send.