Installation and Deployment
About the APM Connect Installation Package
Predix Essentials creates and delivers an installation package that provides the files and folders needed for a successful implementation of APM Connect. This topic describes what may be contained in your installation package based on your requirements.
Contents of the Installation Package
Folder | Description |
---|---|
UDLP - EAM Cloud 3.1.0 Client | Contains the Job Packages for the Cloud Client Installation. |
APM Connect Base 3.0.0 | Contains the APM Connect Base. |
Upgrade the APM Connect Base to V3.0.0
About This Task
The following table outlines the steps that you must complete to upgrade this module to V3.0.0.
These tasks may be completed by multiple people in your organization. However, we recommend that the tasks be completed in the order in which they are listed.
- Because of changes to the Check Connection function, the CMMS_ID and the System Name in the EAM System record must be the same. Before upgrading, make sure you update the EAM System record so these values match.
- If you are using multiple cultures from a single source system, existing data must be updated before you upgrade.
- If you are updating from a significantly older APM Connect version that uses RunDataLoadersRoute.jar to Service the data loader function, the new Service gets renamed to the StageDataLoaderService.jar
Procedure
Upgrade from any version V1.0.0 through V2.0.0
- Uninstall APM Connect.
- Complete the steps to deploy the APM Connect Base for the first time.
Deploy the APM Connect Base for the First Time
The topics outline the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic Predix Essentials system architecture.
About This Task
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
What To Do Next
After deploying the APM Connect Base, deploy any adapters you need.
Run the APM Connect Installer
Before You Begin
Before you can run the APM Connect Installer, you must:
- Ensure that your system meets the APM Connect system requirements.
- Access the APM Connect installation package.
- For SAP integrations, download the SAP Java Connector Files (SAP JCO) from the SAP marketplace.
Procedure
SAP JCO driver installation:
APM Connect set up:
After the progress bar indicates that the APM Connect installer is finishing installation, the Java SE Development Kit installer starts.
Zulu JDK setup:
PostgreSQL setup:
Complete setup:
If you have selected the installation of APM Connect Container service or the SAPJCO driver software , the Administrator: Windows Power Shell and Administrator: Karaf windows appear. Installation progress may not be visible on the screen for 10-15 minutes. During this time, do not press any key or close the windows.Access the APM Connect Administration Center
Using the APM Connect Administration Center, you can run extraction and load jobs. Before you can begin running jobs, you must set up the APM Connect Administration Center. This topic explains how to access and deploy the APM Connect Administration Center for the first time.
Procedure
Restart APM Connect Jobs on Server Reboot
About This Task
Procedure
Update PostgreSQL Networking Configuration
To allow connections from the Predix Essentials Server to APM Connect, you must update the PostgreSQL networking configuration. This topic describes how to perform the configuration update.
Procedure
Results
PostgreSQL is now configured to open the connection from the Predix Essentials Server.
Configure SSL Enabled APM Connect UI (Optional)
About This Task
Procedure
Configure SSL Enabled APM Connect Karaf Services (Optional)
About This Task
Procedure
Results
Configure SSL Enabled APM Connect Karaf Container for SSL Enabled APM (Optional)
Before You Begin
About This Task
If you want to use SSL with Predix Essentials web services, contact GE Global Support.
Procedure
Results
Uninstall APM Connect
Before you can upgrade the APM Connect Base, you must uninstall your current version of APM Connect.