Configure Operations Hub Installation in Interactive Mode
This topic provides step-by-step instructions on how to continue the Operations Hub installation in interactive mode.
Before you begin
Procedure
-
On the welcome screen, select Next.
The license agreement screen appears.
-
Select the Accept check box and select
Next.
The TCP port check screen appears.
-
You need to verify whether the ports for Operations Hub are valid. If not, then
update the ports as necessary.
Note: Use care when changing port numbers to avoid conflict with an existing application. Generally, a port number higher than 1023 should be assigned, since ports 0 to1023 are well known ports typically already assigned on Windows systems for different purposes.
-
Update the field values as described in the following table and select
Next.
Points to consider:
- If Proficy Authentication is already installed, the All Host Names field will be read-only.
- The first entry in the All Host Names field is automatically the primary host name for Proficy Authentication.
- Use the drop-down list to select a different primary host name for Operations Hub.
All Host Names Machine details to access Operations Hub following the install. Choose from: - Fully qualified domain name (FQDN)
- host name
- IP address
Note:- If you want to provide more than one of the aforementioned values, use a comma to separate them.
- If you want to add the Fully Qualified Domain Name (FQDN) after completion of the install, the safest way to apply the FQDN is to uninstall without purge, and then reinstall with the FQDN in the Host Names screen.
Primary Host Name This field remains in a disabled state. It is updated with the first value from All Host Names. Operations Hub Host Name If Proficy Authentication and Operations Hub are installed on the same server, you have the option to configure different domain names. Select a host name from the Operations Hub Host Name drop-down field, ensuring it is different from the host name used when Proficy Authentication was installed.
The Proficy Authentication Service screen appears. -
You have the option to use either an integrated (OR) an external Proficy
Authentication (UAA) service.
-
Update the following tenant admin account field values as described and select
Next.
User Id User ID of the administrator account for Operations Hub. When you provide the tenant user ID, the following conditions apply: - If you are installing Operations Hub for the first time, do not provide StudioAdmin as the tenant user ID because it is used by Operations Hub.
- If you want to use a shared Proficy Authentication to work with Operations Hub, do not provide the user ID of an existing user of the Proficy Authentication instance. If you do so, the installation fails.
- If you are reinstalling Operations Hub, do not provide the tenant user ID that you previously provided. This is because even if you purged the data while uninstalling Operations Hub, the user account, along with the groups and privileges assigned to the user, still exists in the Proficy Authentication instance.
Password Password for the administrator account. Re-enter Password To confirm, re-enter the password for the administrator account. The Select Drive for Programs and Data screen appears. This screen appears only when the host machine has multiple fixed hard drives (step 8).If the host machine has only one drive, then the Customize Log Files and Postgres Data Locations screen appears (step 9).
-
Here, you have the option to specify a different drive for installing
Operations Hub.
-
Enter the following details, and then select Next.
-
Here, you have the option to enable the installation of the Dataflow Editor
tool along with Operations Hub.
-
Update the following field values as described and select
Next.
Base URL Base URL of Configuration Hub container service, such as https://chhost:5000/container-svc/
.Client Id Identifier of a client that has permission (authority) to register with Configuration Hub. Client Secret Client secret that can authenticate the client. -
Select Install to start the installation.