Bullet Graph
Use bullet graphs to compare the performance of any two values.
The horizontal bar in a bullet graph represents the actual value, while the vertical line represents the target value. You can add color-coded range limits to visualize the progression status of the actual value to the target value.
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets (Classic) |
Bullet Graph Properties
Field Name | Description | ||||||
---|---|---|---|---|---|---|---|
Title | Enter a title name for the bullet graph. This name appears at runtime. | ||||||
Engineering Unit | Enter the unit of measurement for values. | ||||||
Display Engineering Unit On Graph | If you select the check box, the specified unit appears next to the horizontal bar that represents the actual value in the graph. Clear the check box to hide the unit. | ||||||
Target Value |
Use any of these options to specify the target and actual values in the
graph:
The bullet graph always compares only a single value against the target value. To compare multiple values, create multiple graphs. When you
drag and drop a query on the bullet graph, only the source value field gets
updated. By default, the source target is set to
|
||||||
Min | Enter the minimum axis value for the graph. | ||||||
Max | Enter the maximum axis value for the graph. | ||||||
Variant | You have an option to use a bar graph instead of the bullet graph.
|
||||||
Number Of Decimals | Enter the number of decimal places to format actual and target values in
the graph. The decimals do not apply to ticks. For example, enter
|
||||||
Width (px) - 0 equals dynamic | Enter the width of the graph in pixels. For example,
600 .If set to |
||||||
Height (px) - 0 equals dynamic | Enter the height of the graph in pixels. For example,
130 . |
||||||
Orientation |
|
||||||
Display EGU on Axis Ticks | Select the check box if you want the engineering unit to appear next to each tick mark value. | ||||||
Display Axis Ticks On Opposite Side | Select the check box if you want the tick marks to appear above the
graph. By default, ticks appear below the graph. |
||||||
Ticks | Choose how to display the tick marks on the graph scale.
|
||||||
Font Color | Select a font color for the graph text. | ||||||
Color | Select a color for the horizontal bar in the graph that represents the actual value. | ||||||
Target Color | Select a color for the vertical line in the graph that represents the target value. | ||||||
Color Background | Select a color to apply as a background for the graph. | ||||||
Custom Limit(s) | Select (+Add Item) to set up custom range limits
and add plot bands to your bullet graph. The plot bands appear in the
background providing a visual display of performance status.
The order of the custom range limit impacts the graph. In the example
figure, the green band represents the first applied range limit (90 -100 %
target) followed by the rest of the range limits as per the order. In bar variant graphs, whenever the value
satisfies a specified range (plot band), the horizontal bar will reflect the
color set for that range. |
||||||
Historian REST Options | Use this property to configure Historian REST queries. You can define
which index of the result set to use as input data. The default
Result Set Index is 0 , wherein the
widget uses the first tag data from the query result set. Enter
1 to consider the second tag data, 2 for
third, so on. Select the Reverse Sorting Order check box to reverse the query result set. The bottom record value is provided as input to the widget. Clear the check box to provide the top record value as input to the widget. |
||||||
Hidden | Select this check box if you want to hide the plug-in. To show the hidden plug-in in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden plug-in. See Page Visuals Tab. |