×
Supercharge your GE solution! Download a free trial of CSense analytics and more.
Create a Field in an Entity
Procedure
- From the main navigation menu, select
ENTITIES.
The
ENTITIES workspace appears.
- Select the entity in which you want to create a field.
A list of fields in the entity appears, along with the data in each field.
- Select Edit Entity Structure.
A list of fields in the entity appears.
- Select Add Field.
A field is created in the entity. By default, the name of the field is Field_1 and the type is String.
- Next to the field name, select , and then modify the name of the field. The name must contain at least one uppercase or lowercase letter.
- In the drop-down list box in the Type column, modify the type of the field if needed.
- Select Save or Save and Exit.
The field is created in the entity.