Pareto Chart
Plot a pareto chart for qualitative analysis of your data.
You can use this widget to run a pareto analysis on your data. A pareto chart is a combination of colums/bars and a line graph. The columns/bars represent individual values, and are arranged in a descending order. The pareto line represents the cumulative total of the values. This visual arrangement helps to identify the most important factors in a given dataset in order to make critical decisions.
The pareto chart widget is available under designing application pages, drag-and-drop GEParetoChart to a container.
. WhenThe following list of properties are specific to this widget. For common properties, refer to Page Components (Classic).
Pareto Chart Properties
Field Name | Description |
---|---|
Name | Enter a title name for the pareto chart. This name helps to identify the pareto chart at runtime. |
Font Size (px) | Set the font size for the title text in pixels. |
Font Color | Select a font color for the pareto chart text. |
Width (px) - 0 equals dynamic | If set to 0, the pareto chart occupies 100% of its container. |
Height (px) | Set a height for the pareto chart in pixels. |
Field Name | Description |
---|---|
Y-Axis Label | Enter a label name for the y-axis. |
X-Axis Label | Enter a label name for the x-axis. |
X-Axis Rotation | Enter the degree of rotation for the x-axis labels. |
Axis Label Font Size (px) | Enter the font size for the axis labels. |
Field Name | Description |
---|---|
Width (px) | Enter a value that defines the thickness of the pareto line in the chart. |
Color | Select a color for the pareto line. |
Hidden | Select this check box if you want to hide the
plug-in. To show the hidden plug-in in Operations Hub new layout, go
to Page Visuals and under
Action column, select ![]() |
Field Name | Description |
---|---|
Variant | Both variants are used to compare two or more values, wherein the length
of the column/bar is proportional to the data value. Select between:
|
Color | Select a color for the columns/bars in the chart. |
Align Tick Marks | Select the check box if you want to align the tick marks on the chart.
So, even if the data being plotted on the right axis (secondary y-axis) exceeds
100%, it will not be displayed above 100%. Instead, the values will be capped
at 100%. If you clear the check box, the tick marks on the left axis (primary y-axis) will allow the right axis (secondary y-axis) to be above 100%. In other words, the right axis (secondary y-axis) will not be tied to the size of the bars on the left axis (primary y-axis). |
Source - Data Source | To provide values for the pareto chart, select the
Query tab to choose from queries that return output
fields for the x-axis and y-axis data:
Note: Currently you can pass values to the widget using a query
only. |