Create a Theme

When you create a theme, it is automatically used in the application that you have selected. You can, however, use a different theme in the application.

  1. In the main navigation menu, select APPS.
    The APPS workspace appears.

  2. In the Name column, select an application.
    The PAGES workspace appears.

  3. In the main navigation menu, select THEME.
    The THEME workspace appears.
  4. Select Create new theme.
    The Create new theme window appears.

  5. Enter a name for the theme, and then select Save. The name must contain at least one uppercase or lowercase letter.
    The workspace for the theme appears, displaying the default settings for each attribute.
  6. As needed, modify the settings, and then select Save theme.
    A message appears, asking you to confirm that you want to use the theme for the application.
  7. Select Yes.
    The theme is created and used in the application.