Have You Seen Operations Hub Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2023 releases, by signing up for one of our upcoming events.
As needed, add fields to the entity.This topic describes how to add a row and enter data manually in an entity. You can also import data from a Microsoft Excel workbook. You cannot, however, add data to baseline entities or pivot entities manually. You can only insert data into these entities using an insert query in an application.
In the main navigation menu, selectENTITIES.
The ENTITIES workspace appears.
Select the entity in which you want to add a row.
Select Add row.
A blank row appears in the table.
Tip: You can add multiple rows together by selecting Add row multiple times.
Enter values in the blank row, and then select Save Changes.
The values that you have entered in the row are saved.
Tip: If you have entered values in multiple rows, but want to save values only for a single row, select in the row.