Custom Plug-In structure
This topic describes how to use plug-in components.
- index.html: Contains the plug-in html code.
- main.js: Contains the plug-in javascript code.
- manifest.json: Contains the plug-in configuration details.
- style.css: Contains the plug-in stylesheet details.
- The scripts folder: Contains external scripts.
Get started with the sample templates to build your own plug-in.
Template Type | How to Use |
---|---|
Download the sample template for simple plug-in Includes examples using data source. |
Use this template to build a simple plug-in.
|
Download the sample template for advanced plug-in
|
Use this template to build an advanced plug-in.
|
The index.html file
JavaScript Dependencies
The easiest way to add external javascript dependencies is to place them in the scripts folder (in the root folder) and reference this dependency in the manifest.json file.
The manifest.json file
Every plug-in must contain a manifest.json file in the root folder of the plug-in. This file provides the essential information about the plug-in to Operations Hub.
manifest.json
file.Parameter | Description |
---|---|
typeName [String] | The unique name of the plug-in. Does not support special characters. For example, comma, period, ampersand, dollar sign, percent sign, parenthesis, asterisk, etc. |
pluginId [String] | The unique ID of the plug-in. The value for this parameter must be a long, random one. |
Type [String] | The type of the plug-in. |
category [String] | The category of the plug-in. |
description [String] | The description of the plug-in. This value appears in Operations Hub when you design an application to include the plug-in. |
info | The following information about the plug-in:
|
scripts [Array] | The array for the scripts that you want to use in the plug-in. |
customIcon [String] | The icon that will appear next to the name of the plug-in in Operations Hub when designing an application to include the plug-in. |
origin [String] | The origin of the plug-in. Provide the value custom for this parameter. |
placeholder [String] | A placeholder for the plug-in, which will appear in Operations Hub when designing an application to include the plug-in. |
preview [String] | The picture preview of the plug-in that will appear in Operations Hub when designing an application to include the plug-in. |
fieldsDescription [Object] | The plug-in description for informational messages. |
isNotAllowToAddFields [Boolean] | Indicates whether to allow the user to add more data fields when designing an application to include the plug-in. If you do not want the user to add data fields, enter true. |
schema{} | An array of the following types of schema:
|
Schema
- Input: The input for a plug-in can be static or dynamic. Static data is available in any of the following JSON schema types:
- string
- number
- integer
- boolean
- null
- object
- array
- Output: The output of a plug-in is defined in the Operations Hub target, such as a query with inputs or a global variable.
Supported Widgets
Field Type | Supported Widgets |
---|---|
Boolean |
|
String |
|
Number |
|
The main.js file
Method | Description |
---|---|
EMBED.getRootElement() | Returns the jqLite element, which must be used as the mounting point of the root element of the plug-in. |
EMBED.onChangeData(callback) | This method is a general data change listener. callback - function, which is invoked with one argument every time when data change event is triggered. |
EMBED.getData() | Returns existing page data. |
Method | Description |
---|---|
EMBED.subscribeFieldToQueryChange(field, callback) | Field object: Data Source Callback: Function that is invoked when query change event received. Callback is invoked with one argument, which is a data selection as per field configuration. |
EMBED.subscribeFieldToGlobalChange(field, callback) | Field object: Data Source Callback: Function that is invoked when global change event received. Callback is invoked with one argument, which is a global data as per field configuration. |
EMBED.subscribeFieldToDataChange(field, callback) | Field object: Data Source Callback: Function that is invoked when global or query change event received. |
EMBED.submitTarget(field, value) | Field object: Data Target Value: javascript primitives or Object/Array This method targets the input of a query or a global variable, as per field configuration. |