Elements of a Page
This topic describes the various elements that you can add to a page and the settings that you can configure.
Elements
- Inputs: Contains UI elements that receive input from application users, such as a button, check box, drop-down list box, slider, toggle, and other elements.
- Display: Contains UI elements that display information in the application, such as plain text, image, graph, map, table, and other elements.
- Layouts: Contains UI elements that are used to create a layout in the page, such as a container, separator, new line, and repeater.
- Tools: Contains UI elements that allow application users to upload an Excel worksheet to load data into an entity, upload a list of devices in a CSV format, or manage events.
- Custom: Contains custom UI plug-in elements that have been uploaded by an application developer.
Settings
Setting | Description |
---|---|
Actions | The action that should be triggered when the element is selected. |
Allow Export | Indicates whether data that appears in the element can be exported. By default, this check box is cleared. |
Conditions | The condition based on which the element appears in the application. For example, you can create a condition that a control button or a warning image be displayed if the temperature recorded by the sensor exceeds 40 degrees Celsius. |
Disabled | Indicates whether you want the element to appear as disabled in the application. |
False Label | The label of the element that should appear when a toggle or an indicator is set to OFF. |
First Option | The first option that appears in an element of the type drop-down list box (for example, select an asset). |
Global Data | Indicates whether the value of the element is available globally for use by other elements or query inputs. This check box is enabled only after you specify an ID for the element. |
Hidden | Indicates whether the element should appear in the application. By default, this check box is cleared. You can configure hidden elements to appear when an action is performed. |
Id | The name of the global variable that will be available if the Global Data check box is selected. |
Label | The label that will appear for elements such as check boxes and drop-down list boxes. |
Maximum | The maximum value for an element that contains a range (such as a slider or a gauge). |
Minimum | The minimum value for an element that contains a range (such as a slider or a gauge). |
Options | Indicates whether the values in the element are hard-coded or displayed dynamically from a query. |
Range Limit | The range of values that application users can enter in the element. |
Required | Indicates whether it is always required to enter a value in the element that is used as an input to a query. By default, this check box is cleared. |
Show <number> rows at a time | The number of rows that can appear at a time in an element of the type grid. |
Show on | The devices in which the element should appear. By default, the options Mobile, Tablet, and Desktop are selected. |
Source | The source from which data should be retrieved to initialize the element. If you are configuring the settings of an input element, you can select one of the following options:
|
Stacked | Indicates whether the bars displayed in an element of the type graph should be stacked. By default, this check box is cleared. |
Step | The step value used for a slider element. |
Style | The style of a meter-type gauge element. |
Target Data | The query input that is the target for the value of the element. |
Tooltips | Indicates whether data in a table cell should contain tooltips displaying the content. By default, this check box is cleared. |
True Label | The label of the element that should appear when a toggle or an indicator is set to ON. |
Type | The data type of an input element. If you are configuring the settings of an element of the type graph or gauge, this field contains a list of graph or gauge types. |
Validation | The validations to be applied on the value entered in an input element. You can select the following options:
|
Width | The width of the element of the type toggle. |
X-axis Label | The label of the horizontal axis of an element of the type graph. |
Y-axis Label | The label of the vertical axis of an element of the type graph. |