About this task
If you want to use or copy an application that was created using a different site, you must export the application, and then import it.Tip: If you want to export multiple applications that use the same entities and queries, export them together (instead of exporting them individually).
Procedure
- In the main navigation menu, select
APPS.
The
APPS workspace appears.
- In the rows containing the applications that you want to export, select the check boxes.
- In the workspace heading, select , and then select Export apps.
A message appears, indicating that the application will be saved in the default download location of the browser.
Tip: Alternatively, in the row containing each application that you want to export, select
, and then select
Export app.
- Select OK.
Each application is exported as a .zip file, which contains:
- a .zip file for each plug-in used in the application.
- an .xml file for the rest of the components used in the application.