Graph
Graphs are data visualizations that you can add to display data in an application.
Note: You need external Internet access to use the graph widget.
Graph Settings
To use a graph widget, in addition to the default settings, you must specify one of the following types of graphs.
Type of Graph | Description | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Bars | Bar graphs show comparison among categories vertically. Specify the following settings for a bar graph:
| ||||||||||||
Columns | Column graphs are similar to bar graphs but are shown vertically instead of horizontally. Specify the following settings for a column graph:
| ||||||||||||
Lines | Line graphs show how data changes over specific intervals of time. Specify the following settings for a line graph:
| ||||||||||||
Pie | In a pie graph, rather than axis points, there is a value that can be set to a query to post data on the pie graph. Specify the following settings for a pie graph:
|
Possible Uses
Graphs are a way to show data visually. For example, if 50 students enrolled for a course, you can use a graph widget to show how their grades have changed over time or it may be beneficial to show what grades the students received by percent.
When you plot the data stored in the M2M Entities using a graph widget, timestamp values are displayed in the following format: hh:mm
Downloading Data from a Graph
You can download data from an entity in a Microsoft Excel worksheet using a graph widget. To do so, in the Graph Properties section, select the Allow Download check box. The download button appears in the upper-right corner of the widget in the application.
Note:
- Downloading occurs based on the query last executed as shown in the graph.
- If the query is executed for the specific date range using Input boxes, for example, data is downloaded based on the condition specified.
- The entity data connected to the graph is downloaded, not the graph itself.
- If multiple queries are connected to the graph, a separate Microsoft Excel worksheet is generated for each query, and it is downloaded in a single worksheet.
- In the time_stamp related fields of the M2M_data Entity, the values of milliseconds are also stored. However, only hour, minute, and second values can be displayed when you use the graph widget.