Rounds Pro Upgrade

Upgrade or Update Rounds Pro to V5.2.2.0.0

Pre-upgrade Steps

The following steps must be completed by Rounds Pro mobile users before the APM server is upgraded.

  1. Ensure all data available on the mobile device is synced with the APM server. This includes all the Readings and Recommendations.
  2. Ensure all Routes Instances are Checked-In.
  3. Logout from the Round Pro mobile app.
  4. Do not login to the app until the APM server upgrade is complete.
  5. After the server upgrade is complete, ensure that you are using the latest version of the Rounds Pro mobile app.

Upgrade Steps

The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.

Upgrade from Upgrade to Procedure
V5.2.xV5.2.2.0.0
V5.1.xV5.2.2.0.0
V5.0.xV5.2.2.0.0
V4.6.2 or a later V4.6.x releaseV5.2.2.0.0
  1. Upgrade from any version V4.6.2.0.0 through V4.6.11.0.0
  2. Upgrade from any version V5.0.1.0.0 through V5.0.7.0.0

Upgrade from any version V5.2.0.0.0 through V5.2.1.0.0

This module will be upgraded to V5.2.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.

Upgrade from any version V5.1.0.0.0 through V5.1.4.0.0

This module will be upgraded to V5.2.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.

Upgrade from any version V5.0.1.0.0 through V5.0.7.0.0

This module will be upgraded to V5.2.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.

Upgrade from any version V4.6.2.0.0 through V4.6.11.0.0

This module will be upgraded to V5.2.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.