Steps
About a Step
Steps are used to monitor assets for a specific condition. Rounds Pro has two types of steps:
- Measurement Locations
- Lubrication Requirements
Note: Site functionality is not fully supported within Rounds Pro. Steps inherit the site for the Asset or FLOC that they are created under. If you do not have access to the assets due to a site access restriction, then any instances that you create from the web or from the mobile application will not contain those steps that exist under the specific assets. If you have a broader site access and create the instance, the steps will be part of the instance and all users will be able to see and update those steps in the Rounds Pro mobile app.
Access a Step
Procedure
Create a Step
Procedure
Results
For more information, refer to the Create a Step Condition section of the documentation for instructions on how to create a condition for a Step.
Copy a Step
Procedure
Results
Note:
- You can copy only a standard step. You cannot copy a step that is associated with a template or a strategy.
- When you copy a conditional step, the details available in the INFORMATION and the LIMITS sections are copied. The copy of the step does not include the details available in the CONDITIONAL STEPS section.