Routes
About Route Creation
Before you can define the Checkpoints that should be addressed along a Route, you must create a Route. The records that you create will depend upon the needs of your company.
Suggested Route Guidelines
When you create a Route, adhere to the following suggested guidelines to ensure optimal operation:
- A single Route should contain no more than 250 Checkpoints.
- A single condition should contain no more than 15 successor Checkpoints.
A Water Bottling Facility
Consider a water bottling facility, which contains a bottling system that consists of the following equipment:
- Filling Machine
- Capping Machine
- Labeling Machine
Assume that each day you want someone to perform a general plant check on each machine in the bottling system. In this case, you might want to create one Route that will be linked to multiple Measurement Locations, identifying detailed checks that should be performed on each piece of equipment. Alternatively, you could create one Route for a General Plant Check Route, which would include a general check of the entire plant. For a Route like this, you might want to include the following Checkpoints:
- Leak check
- Temperature check
- Ink level check
- Vibration check
The instructions in this documentation provide details on creating a Route.
Access a Route
Procedure
Create a Route
Assign a Route to Team Members
You must assign a Route to appropriate team members for the Route to be available to those users in Rounds Data Collection.
About This Task
- To assign a Route to team members, you must be a member of the MI Operator Rounds Administrator or MI Lubrication Management Administrator Security Group, a member of a Security Role that includes one of these groups (that is, MI Health Admin), or a Super User.
- Routes can only be assigned to team members with access to Rounds Data Collection.
- To enhance usability for data collectors, assign to team members only Routes that are relevant to those team members. In other words, APM does not recommend assigning all Routes to all team members.
- For the mobile devices with Windows operating systems, the Download Queries are used to assign users. By default, all Routes are available to all users.Note: Team assignments are not available on Windows Mobile Devices.
Procedure
Results
- When the Route is active and due, or when any Checkpoints on the Route are due or overdue, it will appear in Rounds Data Collection for the specified user(s).
What To Do Next
Activate a Route
Before You Begin
- Fully configure and schedule a Route.
- Assign the Route to the appropriate user(s).
About This Task
Procedure
Reorder Nodes within a Route
About This Task
Checkpoint conditions can be arranged on a route. There are three ways to reorder nodes within a Route:
- Changing the order number
- Drag-and-drop
- Drag-and-drop to the Node Pin Board

Reorder Routes by Changing the Order Number
Procedure
Reorder Nodes within a Route using the Drag-and-Drop Method
Procedure
Reorder Nodes within a Route Using the Node Pin Board
Procedure
Remove a Node from a Route
This topic describes how to remove assets, Checkpoints, and Checkpoint conditions from a Route.
Procedure
- Access the Route from which you want to remove related records.
- In the left pane, select the node representing the asset, Checkpoint, or Checkpoint condition that you want to remove.
- In the left pane, select
, and then select Remove.
Results
- The selected node is removed from the Route. Any removed Checkpoint conditions are deleted from the database. Any removed Checkpoints and related Readings remain in the database. Removing an Equipment or Functional Location from the Route moves all the nodes under that asset node to the Node Pin Board.