Overview Configuration

About Managing Queries

When you select a tab in the Calibration Management Overview page, a query is executed to provide the list of records in the corresponding section. You can, however, change the queries to different ones.

Specify Different Search Queries

About This Task

On the Calibration Management Overview page, when you select the Calibration Queue, Calibration Events, Calibration Profiles, and Calibration Tools tabs in the workspace, the following queries are executed:
  • Calibration Queue Overview: Returns a list of Calibration Queue records. This query is executed when you select Calibration Queue on the Calibration Management Overview page.
  • Calibration Event Asset Context: Returns a list of Calibration Events (also called Calibrations). This query is executed when you select Calibration Events on the Calibration Management Overview page.
  • Applied Template Asset Context: Returns a list of Calibration Profiles that contains templates that have been applied to the assets. This query is executed when you select Calibration Profiles on the Calibration Management Overview page.
  • Calibration Tools Overview: Returns a list of Calibration Tools. This query is executed when you select Calibration Tools on the Calibration Management Overview page.

This topic describes how to specify different search queries for Calibration Management, replacing the default ones.

Procedure

  1. Access the Calibration Admin Preferences page.
  2. In the Overview Configuration workspace, next to the query that you want to replace, select .
    The Select APM Query from the catalog window appears.
  3. Navigate to the folder that contains the query that you want to specify.
  4. Select the query that you want to specify, and then select Open.
    In the box corresponding to the query that you want to replace, the path to the selected query appears.
  5. Repeat steps 3 - 5 for all the other queries that you want to replace.
  6. In the upper-right corner of the Overview Configuration workspace, select Save.
    The default queries are replaced by the queries you selected.

Results

On the Calibration Management Overview page, when you select the tabs in the workspace, the queries that you have specified are executed.

Set the Default Date Range for Calibration Queue

About This Task

This topic describes how to set the default date range for the filter in the Calibration Queue section.

In the Task Next Date Filter Options section, you can modify the date filters that appear in the Calibration Queue section in the Calibration Management Overview page.

Procedure

  1. Access the Calibration Admin Preferences page.
  2. In the Task Next Date Filter Options section in the Overview Configuration section, set the date filters as follows:
    • In the Default column, select the date range that you want to use by default. When you set this filter, the corresponding tasks appear in the Calibration Queue section.
    • In the Display column, select the check boxes for the date ranges that you want to display in the Calibration Queue section. If you select the Custom check box, specify the number of months prior to and after the current date to set the date range filter.
  3. Select Save.
    The tasks in the Calibration Queue section are filtered based on the date range that you have specified. You can set a different date range filter in the Calibration Queue section.