Install and Configure Local Atom
Pre-deployment Checklist
The following table outlines the steps that you must complete prior to deploying and configuring Atom for the first time.
Step | Task |
---|---|
1 | Sign in to the Boomi Platform Account provisioned by GE Vernova. |
2 | Verify system availability for Atom installation, ensuring all necessary configurations are correctly set up. |
3 | Validate access and permissions for both the source and destination systems:
|
4 | Install Postgres database and make required configuration change in the pg_hba.conf file. For more information, see Configure PostgreSQL. |
Set up your environment
About This Task
Procedure
Results
Download Atom Installer
Procedure
Install Atom on Windows
Procedure
What To Do Next
- Open
Services.msc
and validate that the Atom service is installed. - You can view the Atom status by selecting Manage > Atom Management
Note: For more details on the Atom configuration options, refer to the Boomi Documentation available in the Remote Management platform.
Install Integration Pack
Procedure
Results
Attach Environment to an Integration Pack
Procedure
Configure Connection Settings
Procedure
Configure the Context File
Before You Begin
You should have imported the audit job.
About This Task
Procedure
- Navigate to the following folder: C:\APMConnect\Config\<system>.
- Modify ContextFile.xml to indicate the values for your system.
Results
Parameter | Description | Default or Recommended Value |
---|---|---|
CONFIG_FILE_PATH | The path to the context file used for extraction. | Enter your unique value (for example, C:\APMConnect\Config\ContextFile.xml). |
IR_HOST | Intermediary Repository host name. | Enter your unique value. |
IR_DATABASE | Database for the dinoloader job. | Enter your unique value. |
IR_USERID | Intermediary Repository username. | Enter your unique value. |
IR_PASSWORD | Intermediary Repository password. | Enter your unique value. |
IR_SCHEMA | The schema in which the IR database will be created. | The default value is public. |
IR_PORT | Intermediate Repository port. | Default value is 5432. |
APM_USERID | The APM user ID. | Enter your unique value. |
APM_PASSWORD | The APM password. | Enter your unique value. |
APM_DATASOURCE | The name of the APM data source to which the data will be exported. | This is a required parameter. Enter your unique value. |
APM_API_APP_SERVER | The name of the APM API server. | This is a required parameter. Enter your unique value. |
APM_APP_SERVER | The name of the APM server. | This is a required parameter. Enter your unique value. |
TRUSTSTORE_FILE | The directory path to the dinoloader SSL configuration file. | Enter your unique value. |
TRUSTSTORE_PASSWORD | The password for the keystore files. | Enter your unique value. |
USE_SSL | Determines if SSL is used. |
True: will use SSL. False: will not use SSL. |
QUEUE_HOST | The host name of the APM ActiveMQ. | Enter your unique value. |
QUEUE_PORT | APM ActiveMQ port. | Default port is 61616. |
QUEUE_USER | APM ActiveMQ user. | Enter your unique value. |
QUEUE_PASSWORD | APM ActiveMQ password. | Enter your unique value. |
CMMS_ID | Enter your EAM system ID | Enter your unique value. |
Configure PostgreSQL
To allow connections from the APM server to APM Connect, you must update the PostgreSQL networking configuration. This topic describes how to perform the configuration update.
Procedure
Results
What To Do Next
Execute a Process Manually
Procedure
Schedule a Process
Procedure
Stop a Schedule
Procedure
- Sign in to your Boomi Platform Integration page.
- Select Manage and select Atom management.
- Select your Atom and select Deployed Processes.
- Select the dropdown arrow next to the intended process and select Stop Schedules.