Dataloggers in Thickness Monitoring
About Dataloggers in Thickness Monitoring (TM)
Dataloggers are data collection devices, which are used to measure and record the thickness of a component. Using the Thickness Monitoring (TM) module, you can:
- Send data related to a TML to the datalogger.
- Receive data from the datalogger (after you collect measurement data in the field and record it in the datalogger).
Important: If you are using the GE DMS Go/Go+ device and your company restricts the use of removable storage devices in USB ports, the device may not function as expected. You must request an exemption to the company policy from your IT administrator, such that you are allowed Write permissions to the USB drive. Although the Olympus 38DL Plus device supports USB, it does not store its data in the same way and is therefore not likely subject to the same restriction. If your company restricts the use of removable storage devices in USB ports, the datalogger device may not function as expected. You must request an exemption to the company policy from your IT administrator.
The following dataloggers are supported in TM:
- GE DMS Go
- GE DMS Go+
- GE DMS2
- Olympus 37DL Plus Ultrasonic Thickness Gage
- Olympus 38DL Plus Ultrasonic Thickness Gage
- Olympus Epoch 650
For each datalogger, APM provides:
- Baseline Datalogger Mapping records, which are used to send or receive data from the datalogger.
- Default datalogger settings, which you must review and modify if needed before you use the datalogger.
To use dataloggers, you must install the latest version of the GE Device Service as well as any necessary device drivers.
If you have modified the Public\Meridium\Modules\Thickness Monitoring\Queries\TM Assets query, you must revert the query to baseline or add the following SQL code for piping Asset to the query.
[MI Corrosion Analysis Settings].[MI_CA_SET_PIPING_F] "Piping Asset"
Access the TM Dataloggers Page for an Asset or TML Group
About This Task
Procedure
What To Do Next
Access the TM Dataloggers Page for Multiple Assets
About This Task
Procedure
What To Do Next
Modify Datalogger Settings
Before You Begin
- Default datalogger settings are provided by APM. Review these settings prior to making any modifications.
- Datalogger settings are specific to the user, data source, and browser. If you log in as a different user, switch browsers, or use a different data source, you will need to reconfigure your datalogger settings.
- When you send data to a GE DMS Go or GE DMS Go+ datalogger, APM creates a folder in the USB drive. Therefore, you must have the Write permission to the USB drive on the machine that you will use to send data.
- When using the Olympus Epoch 650 device, you must specify the COM port used by the device. Tip: To determine the COM port of the device in Windows:
- Access Device Manager.
- Under Ports (COM & LTP), verify the COM port next to the USB Serial device.
Procedure
Results
What To Do Next
Send Data to a Datalogger
Before You Begin
- Install the GE Device Service on the machine that you will use with dataloggers. If you do not install it, when you attempt to send or receive data, you will be prompted to install it.
- Refer to the limitations when using a datalogger.
- If needed, modify the datalogger settings.
Procedure
Results
If the job is successful, the selected TML records are sent to the device.
If an error occurs, the Datalogger Errors window containing the error messages appears.
If the data related to an asset was already sent to the datalogger previously, a message appears, asking you to confirm whether you want to overwrite the existing data on the datalogger. If you choose to overwrite, the data related to the asset is replaced with the data that you send. If you choose not to overwrite, the data will not be sent to the datalogger.
Receive Data from a Datalogger
Before You Begin
- Install the GE Device Service on the machine that you will use with dataloggers. If you do not install it, when you attempt to send or receive data, you will be prompted to install it.
Procedure
Results
The following analyses are re-calculated:
- TML Corrosion Analysis linked to each TML whose measurement data you have received.
- Asset Corrosion Analysis linked to each asset whose measurement data you have received.