Resources

About Resources

Resources are optional components in a System Reliability Analysis that represent physical parts or materials, such as spare bearings or seals, or human resources, such as mechanics or technicians, that you may want to use within the analysis.

Associating a Resource with an Action or a Risk will create a System Resource Usage Record, which is linked to the appropriate System Action or System Risk record, which will store information that specifics how the resource will be used (e.g., the quantity and duration).

Access a Resource

Procedure

  1. Access the System Reliability Analysis whose resource you want to view.
  2. In the Analysis Summary workspace, select the Resources tab.

    The Resources section appears, displaying a list of resources for the selected System Reliability Analysis.



Delete a Resource

Procedure

  1. Access the Resources section.
  2. Select the row containing the resource that you want to delete, and then select .
    A dialog box with a confirmation message appears.
  3. Select OK.
    The selected resource is deleted.